Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for display.
|
Modifier and Type | Field and Description |
---|---|
static StudioImageCaptureBuilder.UnitsEnumType |
StudioImageCaptureBuilder.UnitsEnumType.INCHES
Use Inched to define resolution
|
static StudioImageCaptureBuilder.UnitsEnumType |
StudioImageCaptureBuilder.UnitsEnumType.MM
Use Millimeters to define resolution
|
static StudioImageCaptureBuilder.UnitsEnumType |
StudioImageCaptureBuilder.UnitsEnumType.PIXELS
Use pixel to define resolution
|
Modifier and Type | Method and Description |
---|---|
StudioImageCaptureBuilder.UnitsEnumType |
StudioImageCaptureBuilder.unitsEnum()
Returns the units enum
License requirements: None. |
static StudioImageCaptureBuilder.UnitsEnumType |
StudioImageCaptureBuilder.UnitsEnumType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioImageCaptureBuilder.UnitsEnumType |
StudioImageCaptureBuilder.UnitsEnumType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioImageCaptureBuilder.UnitsEnumType[] |
StudioImageCaptureBuilder.UnitsEnumType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioImageCaptureBuilder.setUnitsEnum(StudioImageCaptureBuilder.UnitsEnumType unitsEnum)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.