Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for display.
|
Modifier and Type | Field and Description |
---|---|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ANSIA
Use ANSI A drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ANSIB
Use ANSI B drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ANSIC
Use ANSI C drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ANSID
Use ANSI D drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ANSIE
Use ANSI E drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.CUSTOM
Use custom defined drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ISOA0
Use ISO A0 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ISOA1
Use ISO A1 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ISOA2
Use ISO A2 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ISOA3
Use ISO A3 drawing size
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.ISOA4
Use ISO A4 drawing size
|
Modifier and Type | Method and Description |
---|---|
StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.drawingSizeEnum()
Returns the drawing size enum
License requirements: None. |
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StudioImageCaptureBuilder.DrawingSizeEnumType |
StudioImageCaptureBuilder.DrawingSizeEnumType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StudioImageCaptureBuilder.DrawingSizeEnumType[] |
StudioImageCaptureBuilder.DrawingSizeEnumType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StudioImageCaptureBuilder.setDrawingSizeEnum(StudioImageCaptureBuilder.DrawingSizeEnumType drawingSizeEnum)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.