Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for display.
|
Modifier and Type | Field and Description |
---|---|
static ImageBaseBuilder.ReferenceDirection |
ImageBaseBuilder.ReferenceDirection.HORIZONTAL
horizontal reference direction
|
static ImageBaseBuilder.ReferenceDirection |
ImageBaseBuilder.ReferenceDirection.VERTICAL
vertical reference direction
|
Modifier and Type | Method and Description |
---|---|
ImageBaseBuilder.ReferenceDirection |
ImageBaseBuilder.referenceDirectionOption()
Returns the image alignment reference direction type.
|
static ImageBaseBuilder.ReferenceDirection |
ImageBaseBuilder.ReferenceDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImageBaseBuilder.ReferenceDirection |
ImageBaseBuilder.ReferenceDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImageBaseBuilder.ReferenceDirection[] |
ImageBaseBuilder.ReferenceDirection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ImageBaseBuilder.setReferenceDirectionOption(ImageBaseBuilder.ReferenceDirection referenceDirection)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.