Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for display.
|
Modifier and Type | Field and Description |
---|---|
DynamicSectionTypes.ActivePlane |
DynamicSectionBuilder.ActivePlaneData.activeplane |
static DynamicSectionTypes.ActivePlane |
DynamicSectionTypes.ActivePlane.PRIMARY
Primary
|
static DynamicSectionTypes.ActivePlane |
DynamicSectionTypes.ActivePlane.SECONDARY
Secondary
|
Modifier and Type | Method and Description |
---|---|
static DynamicSectionTypes.ActivePlane |
DynamicSectionTypes.ActivePlane.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DynamicSectionTypes.ActivePlane |
DynamicSectionTypes.ActivePlane.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DynamicSectionTypes.ActivePlane[] |
DynamicSectionTypes.ActivePlane.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DynamicSectionBuilder.setActivePlane(DynamicSectionTypes.Axis planeAxis,
DynamicSectionTypes.ActivePlane activePlane)
Sets the active plane in the section
Single Plane: There is no secondary plane. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.