public interface DecalCollection extends TaggedObjectCollection
BasePart
TaggedObjectCollection.Iterator
Modifier and Type | Method and Description |
---|---|
DecalBuilder |
createDecalBuilder(TaggedObject decal)
Creates a
DecalBuilder object if decal is null. |
DecalBuilder |
createDecalBuilderFull(TaggedObject decal)
Creates a
DecalBuilder object with image referenced object if decal is null. |
Decal |
findDecalObject(String journalIdentifier)
Finds the
Decal with the given identifier as recorded in a journal. |
_find_next, iterator
DecalBuilder createDecalBuilder(TaggedObject decal) throws NXException, RemoteException
DecalBuilder
object if decal is null. Otherwise, a Decal object will be edited
decal
- If decal is not null, then this object will be editedNXException
RemoteException
DecalBuilder createDecalBuilderFull(TaggedObject decal) throws NXException, RemoteException
DecalBuilder
object with image referenced object if decal is null. Otherwise, a Decal object will be edited
decal
- If decal is not null, then this object will be editedNXException
RemoteException
Decal findDecalObject(String journalIdentifier) throws NXException, RemoteException
Decal
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
journalIdentifier
- Identifier to be foundNXException
RemoteException
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.