public static class DatumPlaneGridBuilder.GridOrientationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CUSTOM
Grid size, location, and
orientation can be customized
using the manipulator controls
|
static int |
_FROM_DATUM_PLANE
Grid display matches
datum plane display
|
static DatumPlaneGridBuilder.GridOrientationType |
CUSTOM
Grid size, location, and
orientation can be customized
using the manipulator controls
|
static DatumPlaneGridBuilder.GridOrientationType |
FROM_DATUM_PLANE
Grid display matches
datum plane display
|
Modifier and Type | Method and Description |
---|---|
static DatumPlaneGridBuilder.GridOrientationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumPlaneGridBuilder.GridOrientationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumPlaneGridBuilder.GridOrientationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DatumPlaneGridBuilder.GridOrientationType FROM_DATUM_PLANE
public static final DatumPlaneGridBuilder.GridOrientationType CUSTOM
public static final int _FROM_DATUM_PLANE
public static final int _CUSTOM
public static DatumPlaneGridBuilder.GridOrientationType valueOf(int value)
public static DatumPlaneGridBuilder.GridOrientationType valueOf(String name)
public static DatumPlaneGridBuilder.GridOrientationType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.