public static class CgfxMattexBuilder.UseCameraDirectionPlane extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NORMAL_AND_UP_VECTOR
both normal and up vectors are updated based on camera direction
|
static int |
_NORMAL_VECTOR
normal vector is updated based on camera direction
|
static CgfxMattexBuilder.UseCameraDirectionPlane |
NORMAL_AND_UP_VECTOR
both normal and up vectors are updated based on camera direction
|
static CgfxMattexBuilder.UseCameraDirectionPlane |
NORMAL_VECTOR
normal vector is updated based on camera direction
|
Modifier and Type | Method and Description |
---|---|
static CgfxMattexBuilder.UseCameraDirectionPlane |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CgfxMattexBuilder.UseCameraDirectionPlane |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CgfxMattexBuilder.UseCameraDirectionPlane[] |
values()
Returns an array that contains the values for this enum.
|
public static final CgfxMattexBuilder.UseCameraDirectionPlane NORMAL_VECTOR
public static final CgfxMattexBuilder.UseCameraDirectionPlane NORMAL_AND_UP_VECTOR
public static final int _NORMAL_VECTOR
public static final int _NORMAL_AND_UP_VECTOR
public static CgfxMattexBuilder.UseCameraDirectionPlane valueOf(int value)
public static CgfxMattexBuilder.UseCameraDirectionPlane valueOf(String name)
public static CgfxMattexBuilder.UseCameraDirectionPlane[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.