public static class CameraBuilder.StockLens extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_S105
105mm
|
static int |
_S135
135mm
|
static int |
_S210
210mm
|
static int |
_S28
28mm
|
static int |
_S300
300mm
|
static int |
_S35
35mm
|
static int |
_S50
50mm
|
static int |
_S70
70mm
|
static CameraBuilder.StockLens |
S105
105mm
|
static CameraBuilder.StockLens |
S135
135mm
|
static CameraBuilder.StockLens |
S210
210mm
|
static CameraBuilder.StockLens |
S28
28mm
|
static CameraBuilder.StockLens |
S300
300mm
|
static CameraBuilder.StockLens |
S35
35mm
|
static CameraBuilder.StockLens |
S50
50mm
|
static CameraBuilder.StockLens |
S70
70mm
|
Modifier and Type | Method and Description |
---|---|
static CameraBuilder.StockLens |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CameraBuilder.StockLens |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CameraBuilder.StockLens[] |
values()
Returns an array that contains the values for this enum.
|
public static final CameraBuilder.StockLens S28
public static final CameraBuilder.StockLens S35
public static final CameraBuilder.StockLens S50
public static final CameraBuilder.StockLens S70
public static final CameraBuilder.StockLens S105
public static final CameraBuilder.StockLens S135
public static final CameraBuilder.StockLens S210
public static final CameraBuilder.StockLens S300
public static final int _S28
public static final int _S35
public static final int _S50
public static final int _S70
public static final int _S105
public static final int _S135
public static final int _S210
public static final int _S300
public static CameraBuilder.StockLens valueOf(int value)
public static CameraBuilder.StockLens valueOf(String name)
public static CameraBuilder.StockLens[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.