public static class TrimLineDevelopmentBuilder.Convergency extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_HIGH
Onestep solver convergency level is high
|
static int |
_LOW
Onestep solver convergency level is low
|
static int |
_MEDIUM
Onestep solver convergency level is medium
|
static TrimLineDevelopmentBuilder.Convergency |
HIGH
Onestep solver convergency level is high
|
static TrimLineDevelopmentBuilder.Convergency |
LOW
Onestep solver convergency level is low
|
static TrimLineDevelopmentBuilder.Convergency |
MEDIUM
Onestep solver convergency level is medium
|
Modifier and Type | Method and Description |
---|---|
static TrimLineDevelopmentBuilder.Convergency |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TrimLineDevelopmentBuilder.Convergency |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TrimLineDevelopmentBuilder.Convergency[] |
values()
Returns an array that contains the values for this enum.
|
public static final TrimLineDevelopmentBuilder.Convergency LOW
public static final TrimLineDevelopmentBuilder.Convergency MEDIUM
public static final TrimLineDevelopmentBuilder.Convergency HIGH
public static final int _LOW
public static final int _MEDIUM
public static final int _HIGH
public static TrimLineDevelopmentBuilder.Convergency valueOf(int value)
public static TrimLineDevelopmentBuilder.Convergency valueOf(String name)
public static TrimLineDevelopmentBuilder.Convergency[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.