public static class SpringbackCompensationBuilder.DegreeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIVE
Degree is 5
|
static int |
_SEVEN
Degree is 7
|
static int |
_THREE
Degree is 3
|
static int |
_TWO
Degree is 2
|
static SpringbackCompensationBuilder.DegreeType |
FIVE
Degree is 5
|
static SpringbackCompensationBuilder.DegreeType |
SEVEN
Degree is 7
|
static SpringbackCompensationBuilder.DegreeType |
THREE
Degree is 3
|
static SpringbackCompensationBuilder.DegreeType |
TWO
Degree is 2
|
Modifier and Type | Method and Description |
---|---|
static SpringbackCompensationBuilder.DegreeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SpringbackCompensationBuilder.DegreeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SpringbackCompensationBuilder.DegreeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SpringbackCompensationBuilder.DegreeType TWO
public static final SpringbackCompensationBuilder.DegreeType THREE
public static final SpringbackCompensationBuilder.DegreeType FIVE
public static final SpringbackCompensationBuilder.DegreeType SEVEN
public static final int _TWO
public static final int _THREE
public static final int _FIVE
public static final int _SEVEN
public static SpringbackCompensationBuilder.DegreeType valueOf(int value)
public static SpringbackCompensationBuilder.DegreeType valueOf(String name)
public static SpringbackCompensationBuilder.DegreeType[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.