public static class FingerClearanceNotchBuilder.Types extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FACE
Build from either a single face or a set of connected faces.
|
static int |
_SECTION
Build from an open section profile.
|
static int |
_SHEET_BODY
Build from either a sheet body or a solid body.
|
static FingerClearanceNotchBuilder.Types |
FACE
Build from either a single face or a set of connected faces.
|
static FingerClearanceNotchBuilder.Types |
SECTION
Build from an open section profile.
|
static FingerClearanceNotchBuilder.Types |
SHEET_BODY
Build from either a sheet body or a solid body.
|
Modifier and Type | Method and Description |
---|---|
static FingerClearanceNotchBuilder.Types |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FingerClearanceNotchBuilder.Types |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FingerClearanceNotchBuilder.Types[] |
values()
Returns an array that contains the values for this enum.
|
public static final FingerClearanceNotchBuilder.Types SECTION
public static final FingerClearanceNotchBuilder.Types FACE
public static final FingerClearanceNotchBuilder.Types SHEET_BODY
public static final int _SECTION
public static final int _FACE
public static final int _SHEET_BODY
public static FingerClearanceNotchBuilder.Types valueOf(int value)
public static FingerClearanceNotchBuilder.Types valueOf(String name)
public static FingerClearanceNotchBuilder.Types[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.