public static class DrawBeadBuilder.OrientationTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ORTHOGONAL
The width and angle parameters are orthogonal, or normal, to the sheet metal normal at the section location.
|
static int |
_VERTICAL
The width and angle parameters are oriented along the draw direction at the section location.
|
static DrawBeadBuilder.OrientationTypes |
ORTHOGONAL
The width and angle parameters are orthogonal, or normal, to the sheet metal normal at the section location.
|
static DrawBeadBuilder.OrientationTypes |
VERTICAL
The width and angle parameters are oriented along the draw direction at the section location.
|
Modifier and Type | Method and Description |
---|---|
static DrawBeadBuilder.OrientationTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DrawBeadBuilder.OrientationTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DrawBeadBuilder.OrientationTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final DrawBeadBuilder.OrientationTypes ORTHOGONAL
public static final DrawBeadBuilder.OrientationTypes VERTICAL
public static final int _ORTHOGONAL
public static final int _VERTICAL
public static DrawBeadBuilder.OrientationTypes valueOf(int value)
public static DrawBeadBuilder.OrientationTypes valueOf(String name)
public static DrawBeadBuilder.OrientationTypes[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.