public class DieBuildStatusOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FAIL
Sub feature build has failed.
|
static int |
_INDETERMINANT
Build status could not be determined since sub feature is not active.
|
static int |
_UNKNOWN
Build status is unknown since sub feature has not been built yet.
|
static int |
_VALID
Sub feature has built successfully.
|
static DieBuildStatusOption |
FAIL
Sub feature build has failed.
|
static DieBuildStatusOption |
INDETERMINANT
Build status could not be determined since sub feature is not active.
|
static DieBuildStatusOption |
UNKNOWN
Build status is unknown since sub feature has not been built yet.
|
static DieBuildStatusOption |
VALID
Sub feature has built successfully.
|
Modifier and Type | Method and Description |
---|---|
static DieBuildStatusOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DieBuildStatusOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DieBuildStatusOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final DieBuildStatusOption INDETERMINANT
public static final DieBuildStatusOption UNKNOWN
public static final DieBuildStatusOption FAIL
public static final DieBuildStatusOption VALID
public static final int _INDETERMINANT
public static final int _UNKNOWN
public static final int _FAIL
public static final int _VALID
public static DieBuildStatusOption valueOf(int value)
public static DieBuildStatusOption valueOf(String name)
public static DieBuildStatusOption[] values()
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.