Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Polyline
Represents a polyline curve.
|
Modifier and Type | Field and Description |
---|---|
Spline |
SelectSpline.ValueData.selection
selected object
|
Spline |
SelectSpline.ValueWithCaeSetObjectInfoData.selection
selected object
|
Spline |
SelectSpline.ValueWithSnapData.selection1
first selected object
|
Spline |
SelectSpline.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
Spline |
SplineCollection.findObject(String journalIdentifier)
Finds the
Spline with the given identifier as recorded in a journal. |
Spline[] |
SelectSplineList.getArray()
Returns the list of objects in the selection list.
|
Spline |
SketchG2Constraint.spline()
Returns the spline on which the G2 constraint is applied.
|
Spline |
SketchG1Constraint.spline()
Returns the spline on which the G1 constraint is applied.
|
Spline |
SelectSpline.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
boolean |
SelectSplineList.add(Spline object)
Adds an object to the list
License requirements: None. |
boolean |
SelectSplineList.add(Spline[] objects)
Adds a set of objects to the list
License requirements: None. |
boolean |
SelectSplineList.add(Spline selection,
View view,
Point3d point)
Adds the object with the objects view and objects point
License requirements: None. |
boolean |
SelectSplineList.contains(Spline object)
Returns whether the specified object is already in the list or not.
|
void |
Sketch.convertToNx10Spline(Spline spline)
Convert the legacy splines to new NX10 splines.
|
void |
Sketch.editSplineDefiningPoints(Spline spline,
double[] points)
Changes the locations of the defining points of a spline.
|
void |
Sketch.editSplinePoles(Spline spline,
double[] poles)
Changes the locations of the control poles of a spline.
|
boolean |
SelectSplineList.remove(InferSnapType.SnapType snapType,
Spline selection1,
View view1,
Point3d point1,
Spline selection2,
View view2,
Point3d point2)
Remove specified object from list.
|
boolean |
SelectSplineList.remove(Spline object)
Remove specified object from list.
|
boolean |
SelectSplineList.remove(Spline object,
View view)
Remove specified object from list.
|
boolean |
SelectSplineList.removeArray(Spline[] objects)
Remove specified objects from list.
|
void |
SelectSplineList.setArray(Spline[] objects)
Sets the list of objects in the selection list.
|
void |
SelectSpline.setValue(Spline selection)
Sets the object being selected
License requirements: None. |
void |
SelectSpline.setValue(Spline selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
boolean |
SelectSplineList.setValueWithCaeSetObjectInfo(Spline selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObjectList.add(nxopen.TaggedObject) .
|
void |
SelectSpline.setValueWithCaeSetObjectInfo(Spline selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
boolean |
SelectSplineList.setValueWithSnap(InferSnapType.SnapType snapType,
Spline selection1,
View view1,
Point3d point1,
Spline selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
void |
SelectSpline.setValueWithSnap(InferSnapType.SnapType snapType,
Spline selection1,
View view1,
Point3d point1,
Spline selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Modifier and Type | Method and Description |
---|---|
RelatedNodeMethod |
SmartSelectionManager.createRelatedNodeMethod(Spline[] seedTags)
Creates a related node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
Spline[] |
FeatureExtractionBuilder.getExtractedBorders()
Gets the extracted curves.
|
Modifier and Type | Method and Description |
---|---|
Spline |
RapidSurfaceBuilder.askEdge(int edgeIndex)
Asks an edge in the current curve network
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Spline |
StudioSplineBuilderEx.curve()
Returns the spline curve
License requirements: None. |
Spline |
StudioSplineBuilder.curve()
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
Modifier and Type | Method and Description |
---|---|
DraftingSplineBuilder |
FeatureCollection.createDraftingSplineBuilder(Spline spline)
Creates a Studio Spline builder for drafting
License requirements: features_modeling ("FEATURES MODELING"), solid_modeling ("SOLIDS MODELING") . |
SketchSplineBuilder |
FeatureCollection.createSketchSplineBuilder(Spline spline)
Creates a Studio Spline builder for sketcher
License requirements: features_modeling ("FEATURES MODELING") OR geometric_tol ("GDT"), solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
TrimCurveBuilder |
FeatureCollection.createTrimCurveBuilder(Spline trimCurve)
Creates a
TrimCurveBuilder
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") Created in NX7.5.0 |
void |
StudioSplineBuilder.setNonParametricSpline(Spline spline,
StudioSplineBuilder.Method method)
Deprecated.
Deprecated in NX8.0.0. Use
StudioSplineBuilderEx instead.
|
Modifier and Type | Method and Description |
---|---|
void |
CurveShapingBuilder.deleteAllPoints(Spline curve)
Deletes all points on a curve.
|
Modifier and Type | Interface and Description |
---|---|
interface |
SplineSegment
Represents a spline segment.
|
Modifier and Type | Field and Description |
---|---|
Spline |
SBendCornerCollection.ComputeSBendData.bendCurve
S-Bend spline when a valid solution exists;
null otherwise.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.