Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SketchChamferBuilder.ChamferOptions |
SketchChamferBuilder.ChamferOptions.ASYMMETRIC
Asymmetric - specify two distances
|
static SketchChamferBuilder.ChamferOptions |
SketchChamferBuilder.ChamferOptions.OFFSETAND_ANGLE
OffsetandAngle - specify offset distance and angle
|
static SketchChamferBuilder.ChamferOptions |
SketchChamferBuilder.ChamferOptions.SYMMETRIC
Symmetric - specify one distance
|
Modifier and Type | Method and Description |
---|---|
SketchChamferBuilder.ChamferOptions |
SketchChamferBuilder.chamferOption()
Returns the chamfer options that specify what type of chamfer is to be created
License requirements: drafting ("DRAFTING") OR solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
static SketchChamferBuilder.ChamferOptions |
SketchChamferBuilder.ChamferOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchChamferBuilder.ChamferOptions |
SketchChamferBuilder.ChamferOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchChamferBuilder.ChamferOptions[] |
SketchChamferBuilder.ChamferOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchChamferBuilder.setChamferOption(SketchChamferBuilder.ChamferOptions chamferOption)
License requirements: drafting ("DRAFTING") OR solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.