Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SketchAlongPathBuilder.SketchOrientationType |
SketchAlongPathBuilder.SketchOrientationType.AUTOMATIC
Automatic
|
static SketchAlongPathBuilder.SketchOrientationType |
SketchAlongPathBuilder.SketchOrientationType.RELATIVE_TO_FACE
Relative to face
|
static SketchAlongPathBuilder.SketchOrientationType |
SketchAlongPathBuilder.SketchOrientationType.USE_CURVE_PARAMETERS
Based on curve parameter
|
Modifier and Type | Method and Description |
---|---|
SketchAlongPathBuilder.SketchOrientationType |
SketchAlongPathBuilder.sketchOrient()
Returns the sketch orientation method as
SketchAlongPathBuilder.SketchOrientationType
License requirements: None. |
static SketchAlongPathBuilder.SketchOrientationType |
SketchAlongPathBuilder.SketchOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchAlongPathBuilder.SketchOrientationType |
SketchAlongPathBuilder.SketchOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchAlongPathBuilder.SketchOrientationType[] |
SketchAlongPathBuilder.SketchOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchAlongPathBuilder.setSketchOrient(SketchAlongPathBuilder.SketchOrientationType sketchOrientMethod)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.