Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static SketchAlongPathBuilder.PlaneOrientationType |
SketchAlongPathBuilder.PlaneOrientationType.NORMAL_TO_PATH
Normal to Path
|
static SketchAlongPathBuilder.PlaneOrientationType |
SketchAlongPathBuilder.PlaneOrientationType.NORMAL_TO_VECTOR
Normal to Vector
|
static SketchAlongPathBuilder.PlaneOrientationType |
SketchAlongPathBuilder.PlaneOrientationType.PARALLEL_TO_VECTOR
Parallel to Vector
|
static SketchAlongPathBuilder.PlaneOrientationType |
SketchAlongPathBuilder.PlaneOrientationType.THROUGH_AXIS
Through Axis
|
Modifier and Type | Method and Description |
---|---|
SketchAlongPathBuilder.PlaneOrientationType |
SketchAlongPathBuilder.planeOrientation()
Returns the plane orientation type
License requirements: None. |
static SketchAlongPathBuilder.PlaneOrientationType |
SketchAlongPathBuilder.PlaneOrientationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchAlongPathBuilder.PlaneOrientationType |
SketchAlongPathBuilder.PlaneOrientationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchAlongPathBuilder.PlaneOrientationType[] |
SketchAlongPathBuilder.PlaneOrientationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchAlongPathBuilder.setPlaneOrientation(SketchAlongPathBuilder.PlaneOrientationType planeOrientationType)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.