Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Method and Description |
---|---|
Sketch.ConstraintGeometry[] |
SketchGeometricConstraint.getGeometry()
Returns the geometry associated with the constraint
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SketchGeometricConstraint |
Sketch.createCoincidentConstraint(Sketch.ConstraintGeometry geom1,
Sketch.ConstraintGeometry geom2)
Creates a coincident constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createCollinearConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a collinear constraint.
|
SketchGeometricConstraint |
Sketch.createConcentricConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a concentric constraint.
|
SketchGeometricConstraint |
Sketch.createConstantAngleConstraint(Sketch.ConstraintGeometry conGeom)
Creates a constant angle constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createConstantLengthConstraint(Sketch.ConstraintGeometry conGeom)
Creates a constant length constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createEqualLengthConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates an equal length constraint.
|
SketchGeometricConstraint |
Sketch.createEqualRadiusConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates an equal radius constraint.
|
SketchGeometricConstraint |
Sketch.createFixedConstraint(Sketch.ConstraintGeometry geom)
Creates a fixed constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint[] |
Sketch.createFullyFixedConstraints(Sketch.ConstraintGeometry geom)
Creates enough fixed constraints on the curve and all of its vertices such that the geometry is fully
fixed without any redundant fixed constraints.
|
SketchGeometricConstraint |
Sketch.createHorizontalConstraint(Sketch.ConstraintGeometry geom)
Creates a horizontal constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createMidpointConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a midpoint constraint.
|
SketchGeometricConstraint |
Sketch.createNonUniformScaledConstraint(Sketch.ConstraintGeometry conGeom)
Creates a non-uniform scale constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createNormalConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometryHelp geom1Help,
Sketch.ConstraintGeometry conGeom2,
Sketch.ConstraintGeometryHelp geom2Help)
Creates a normal constraint.
|
SketchGeometricConstraint |
Sketch.createParallelConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a parallel constraint.
|
SketchGeometricConstraint |
Sketch.createPerpendicularConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a perpendicular constraint.
|
SketchHelpedGeometricConstraint |
Sketch.createPointOnCurveConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2,
Sketch.ConstraintGeometryHelp help)
Creates a point on curve constraint.
|
SketchHelpedGeometricConstraint |
Sketch.createPointOnStringConstraint(Sketch.ConstraintGeometry conGeom1,
Curve[] curvesInString,
Sketch.ConstraintGeometryHelp helpData,
int curveWhichHelpParamAppliesTo)
Creates a point on string constraint.
|
SketchHelpedGeometricConstraint |
Sketch.createPointOnStringConstraint(Sketch.ConstraintGeometry conGeom1,
Curve curveInString,
Sketch.ConstraintGeometryHelp helpData)
Creates a point on string constraint.
|
SketchGeometricConstraint |
Sketch.createSlopeConstraint(Sketch.ConstraintGeometry conGeom1,
Sketch.ConstraintGeometry conGeom2)
Creates a slope constraint.
|
SketchTangentConstraint |
Sketch.createTangentConstraint(Sketch.ConstraintGeometry geom1,
Sketch.ConstraintGeometryHelp geom1Help,
Sketch.ConstraintGeometry geom2,
Sketch.ConstraintGeometryHelp geom2Help)
Creates a tangent constraint.
|
SketchGeometricConstraint |
Sketch.createUniformScaledConstraint(Sketch.ConstraintGeometry conGeom)
Creates a uniform scale constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
SketchGeometricConstraint |
Sketch.createVerticalConstraint(Sketch.ConstraintGeometry geom)
Creates a vertical constraint
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
Sketch.deleteConstraintsOnGeometries(Sketch.ConstraintGeometry[] objects)
Deletes all geometric constraints associated with the object and all of its vertices.
|
void |
Sketch.hideDimensions(Sketch.ConstraintGeometry[] objects)
Blanks dimensions in the active sketch associated with the input sketch geometry.
|
void |
Sketch.showDimensions(Sketch.ConstraintGeometry[] objects)
Unblanks dimensions in the active sketch associated with the input sketch geometry.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.