Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.AutoDimensioningRule |
Sketch.AutoDimensioningRule.ADJACENT_ANGLE
Create Adjacent Angles
|
static Sketch.AutoDimensioningRule |
Sketch.AutoDimensioningRule.HORIZONTAL_VERTICAL
Create Horizontal and Vertical Dimensions
|
static Sketch.AutoDimensioningRule |
Sketch.AutoDimensioningRule.LENGTH
Create Length Dimension
|
static Sketch.AutoDimensioningRule |
Sketch.AutoDimensioningRule.REFERENCE_AXES
Create Dimensions to Reference Axes
|
static Sketch.AutoDimensioningRule |
Sketch.AutoDimensioningRule.SYMMETRIC
Create Symmetric Dimensions
|
Modifier and Type | Method and Description |
---|---|
Sketch.AutoDimensioningRule[] |
SketchAutoDimensionBuilder.getRules()
Get the auto dimensioning rule list from builder
License requirements: None. |
Sketch.AutoDimensioningRule[] |
InferredConstraintsBuilder.getRules()
Get the auto dimensioning rule list into an array
License requirements: None. |
static Sketch.AutoDimensioningRule |
Sketch.AutoDimensioningRule.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.AutoDimensioningRule |
Sketch.AutoDimensioningRule.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.AutoDimensioningRule[] |
Sketch.AutoDimensioningRule.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SketchAutoDimensionBuilder.setRules(Sketch.AutoDimensioningRule[] rules)
Set the auto dimensioning rule list to builder.
|
void |
InferredConstraintsBuilder.setRules(Sketch.AutoDimensioningRule[] rules)
Set the auto dimensioning rule list to builder
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.