Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Method and Description |
---|---|
SelectFace |
CoplanarBuilder.constraintFace()
Returns the face change
License requirements: None. |
SelectFace |
VariableOffsetBuilder.face()
Returns the face to be offset
License requirements: None. |
SelectFace |
PartGeometryCopySelectBuilder.face()
Returns the face
License requirements: None. |
SelectFace |
EnlargeBuilder.face()
Returns the face
License requirements: nx_freeform_2 ("advanced freeform modeling") . |
SelectFace |
TangentBuilder.motionFace()
Returns the motion face
License requirements: None. |
SelectFace |
SymmetricBuilder.motionFace()
Returns the motion face.
|
SelectFace |
PerpendicularBuilder.motionFace()
Returns the motion face
License requirements: None. |
SelectFace |
ParallelBuilder.motionFace()
Returns the motion face.
|
SelectFace |
MakeOffsetBuilder.motionFace()
Returns the motion face
License requirements: None. |
SelectFace |
CoaxialBuilder.motionFace()
Returns the motion face.
|
SelectFace |
ShowRelatedFacesBuilder.relatedFace()
Returns the related face
License requirements: None. |
SelectFace |
ReplaceFaceBuilder.replacementFace()
Returns the replacement face, only for replace type, don't use it until nx502
License requirements: None. |
SelectFace |
PatchBuilder.seedFace()
Returns the seed face.
|
SelectFace |
ExtractFaceBuilder.seedFace()
Returns the seed face for the face chain
License requirements: None. |
SelectFace |
PointSetBuilder.singleFaceObject()
Returns the select object that is used to hold the face.
|
SelectFace |
SymmetricBuilder.stationaryFace()
Returns the stationary face.
|
SelectFace |
MakeOffsetBuilder.stationaryFace()
Returns the stationary face
License requirements: None. |
SelectFace |
SnipSurfaceBuilder.targetFace()
Returns the target face
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
SelectFace |
PoleSmoothingBuilder.targetFace()
Returns the target face
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Method and Description |
---|---|
SelectFace |
ResizeBendAngleBuilder.bendFace()
Returns the bend face
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
SelectFace |
GussetBuilder.bendFace()
Returns the bend face
Selects the bend face along which the gusset is placed. |
SelectFace |
AeroLighteningCutoutBuilder.holeFace()
Returns the hole face
License requirements: None. |
SelectFace |
ResizeBendAngleBuilder.referenceFace()
Returns the reference face
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
SelectFace |
FlatSolidBuilder.stationaryFace()
Returns the stationary face selection
License requirements: None. |
SelectFace |
SolidPunchBuilder.targetFace()
Returns the target face
License requirements: None. |
SelectFace |
FlatPatternBuilder.upwardFace()
Returns the upward face selection
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectFace |
WeldCut2Builder.cornerTargetFace()
Returns the corner target face.
|
SelectFace |
WeldCut2Builder.csystargetFace()
Returns the csys target face.
|
SelectFace |
WeldCut2Builder.curveTargetFace()
Returns the curve target face.
|
SelectFace |
WeldCutBuilder.selectCSYSFace()
Returns the selection object for the target face.
|
SelectFace |
ShipCutoutBuilder.selectCSYSFace()
Returns the selection object for the target face.
|
SelectFace |
SteelCollarPlateBuilder.selectFace()
Returns the select face.
|
SelectFace |
ExcessMaterialBuilder.selectFace()
Deprecated.
Deprecated in NX8.0.0. Use
ExcessMaterialBuilder.selectFaces() instead.
|
SelectFace |
WeldCutBuilder.selectTargetFace()
Returns the selection object for the target face.
|
Modifier and Type | Method and Description |
---|---|
SelectFace |
SnipIntoPatchesBuilder.face()
Returns the face to snip into patches
License requirements: None. |
SelectFace |
LocalUntrimBuilder.face()
Returns the tool object to split the target body.
|
SelectFace |
BridgeCurveConnectivity.perpendicularFace()
Returns the perpendicular face
License requirements: None. |
SelectFace |
MatchSurfaceBuilder.referenceFace()
Returns the selected face for reference curve
License requirements: None. |
SelectFace |
EndHoleData.untilSelectedTarget()
Returns the until selected target - this is applicable for general hole and threaded hole type
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectFace |
BlankGeneratorBuilder.datumFace()
Returns the face used to update a blank.
|
SelectFace |
ElectrodeInitializationBuilder.face()
Returns the face whose center will be the origin of the machine set csys.
|
SelectFace |
ElectrodeComponentBuilder.face()
Returns the face whose center will be the origin of the machine set csys.
|
SelectFace |
MWMoldedPartValidationBuilder.informationInspectFace()
Returns the face selected face for displaying the face properties.
|
SelectFace |
WallThicknessCheckerBuilder.inspectionDynamicPointOnFace()
Returns the selected location on face for displaying dynamic thickness display
License requirements: None. |
SelectFace |
ElectrodeBlankBuilder.jointFace()
Returns the face to create a joint object between the blank and head bodies.
|
SelectFace |
BlankGeneratorBuilder.stationaryFace()
Returns the face used to create a blank.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.