Package | Description |
---|---|
nxopen.bodydes |
Provides classes and interfaces for Body Design.
|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.features.vehicledesign |
Provides classes and interfaces for the Vehicle Design.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Method and Description |
---|---|
SelectBodyList |
OnestepUnformBuilder.unfoldSolidRegion()
Returns the unfold solid regions which are a group of faces user chooses to unform.
|
Modifier and Type | Method and Description |
---|---|
SelectBodyList |
SurfaceRegions.bodies()
Returns the bodies
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectBodyList |
QuickBinderWrapBuilder.button()
Returns the button
License requirements: None. |
SelectBodyList |
ClearanceBuilder.geometry()
Returns the solid to use for the basis of the clearance area.
|
SelectBodyList |
CompensateRoughDataBuilder.sheetBodies()
Returns the sheet bodies that will be approximated.
|
Modifier and Type | Method and Description |
---|---|
SelectBodyList |
PromotionBuilder.body()
Returns the body to be promoted
License requirements: None. |
SelectBodyList |
MidSurfaceByFacePairsBuilder.bodySelection()
Returns the solid bodies for midsurface definition
License requirements: None. |
SelectBodyList |
ScaleBuilder.bodyToScale()
Returns the bodyToScale
License requirements: None. |
SelectBodyList |
MirrorBodyBuilder.mirrorBodyList()
Deprecated.
Deprecated in NX9.0.0. Use
MirrorBodyBuilder.mirrorBodyCollector() instead.
|
SelectBodyList |
MidSurfaceUserDefinedBuilder.sheetBodySelection()
Returns the sheet bodies to be treated as user defined neutral sheets
License requirements: None. |
SelectBodyList |
MidSurfaceByFacePairsBuilder.sheetSelection()
Returns the user defined sheet selection
License requirements: None. |
SelectBodyList |
SplitBodyBuilder.targetBody()
Returns the target body to split.
|
SelectBodyList |
AssemblyCutBuilder.targetBody()
Returns the target body
License requirements: None. |
SelectBodyList |
BooleanBuilder.targets()
Returns the target bodies for the boolean operation
License requirements: None. |
SelectBodyList |
PasteFaceBuilder.toolBody()
Returns the collector holding the tool bodies.
|
SelectBodyList |
AssemblyCutBuilder.toolBody()
Returns the tool body
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectBodyList |
PlateBuilder.adoptionBodies()
Returns the adoption bodies, which are used to create multiple plates.
|
SelectBodyList |
PlateBuilder.bodyBoundary()
Returns the body boundary, which can be mixed with curve, face and plane to define the plate boundary.
|
SelectBodyList |
ShipProfileCutoutBuilder.profileBodies()
Returns the profile bodies
License requirements: None. |
SelectBodyList |
InverseBendingLinesBuilder.profileBodies()
Returns the profile bodies to create Inverse Bending Lines on.
|
SelectBodyList |
AlongGuideCutBuilder.shipStructure()
Returns the target plate or stiffener when the
AlongGuideCutBuilder.CreationMethod
is AlongGuideCutBuilder.CreationMethod.WELD_CLEARANCE . |
SelectBodyList |
SteelDistributionBuilder.steelBodies()
Returns the steel bodies
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectBodyList |
TireEnvelopeBuilder.clearanceAnalysisBodies()
Returns the selection list containing the solid objects used in the clearance analysis.
|
SelectBodyList |
TireEnvelopeBuilder.tireDefinitionBody()
Returns the selection list for tire body.
|
Modifier and Type | Method and Description |
---|---|
SelectBodyList |
LayoutManagementBuilder.bodiesReposition()
Returns the select bodies to reposition
License requirements: None. |
SelectBodyList |
InitProjectBuilder.bodySelect()
Returns the body will be used as product to create Mold Wizard project
License requirements: None. |
SelectBodyList |
ChannelFittingBuilder.boundaryBody()
Returns the boundary body to create the cooling fitting points.
|
SelectBodyList |
ScrapDesignBuilder.changeColScrap()
Returns the changing color of scrap
License requirements: None. |
SelectBodyList |
SpecifyBaffleBuilder.channels()
Returns the channel or body to assign new attributes.
|
SelectBodyList |
MotionSimulationBuilder.component()
Returns the component to assign die components mounted to a kinematic component.
|
SelectBodyList |
ReliefDesignBuilder.copyRelief()
Returns the relief used to copy.
|
SelectBodyList |
InsertAuxiliaryBuilder.copySelectInsert()
Returns the insert to be copied.
|
SelectBodyList |
DieBaseBuilder.dieBaseToDelete()
Returns the selected die base to delete.
|
SelectBodyList |
ScrapDesignBuilder.existScrap()
Returns the existed scrap served for exist sheet body method
License requirements: None. |
SelectBodyList |
CoolingExtendBuilder.extendChannel()
Returns the cooling channel to be extended.
|
SelectBodyList |
EWMultiPositionBuilder.head()
Returns the head to match to another possible head.
|
SelectBodyList |
ElectrodeBlankBuilder.headBodies()
Returns the head bodies to be used to create a blank.
|
SelectBodyList |
SpecifyCircuitBuilder.inletChannel()
Returns the inlet channel.
|
SelectBodyList |
InsertAuxiliaryBuilder.insertsToDelete()
Returns the insert objects to be deleted.
|
SelectBodyList |
ElectrodeCopyBuilder.mirrorPlane()
Returns the mirror plane
License requirements: None. |
SelectBodyList |
PiercingInsertBuilder.normalSelectPierceDieInsert()
Returns the select pierce die insert to be edited.
|
SelectBodyList |
PiercingInsertBuilder.normalSelectPiercePunch()
Returns the select pierce punch insert to be edited.
|
SelectBodyList |
ChannelFittingBuilder.parentChannel()
Returns the parent channel of the cooling fitting points.
|
SelectBodyList |
SolidPatchBuilder.patch()
Returns the tool bodies selected as linked source bodies for patching up the target body.
|
SelectBodyList |
AssignPatchBuilder.patchSurfaces()
Returns the selected surfaces added as patch surfaces or deleted from patch surfaces.
|
SelectBodyList |
RunnerBuilder.runnerBodies()
Returns the runner bodies
License requirements: None. |
SelectBodyList |
ScrapDesignBuilder.secondScrap()
Returns the second scrap to merge with the first one
License requirements: None. |
SelectBodyList |
PiercingInsertBuilder.selectAssociationInsert()
Returns the selection of the inserts to create association.
|
SelectBodyList |
PiercingInsertBuilder.selectAssociationScrap()
Returns the selection of the scrap to create association.
|
SelectBodyList |
ProfileSplitBuilder.selectBody()
Returns the selected body to be splitted
License requirements: None. |
SelectBodyList |
MoldInsertBuilder.selectBody()
Returns the select body
License requirements: None. |
SelectBodyList |
SubInsertBuilder.selectBotFace()
Returns the bottom face to position the sub-insert
License requirements: None. |
SelectBodyList |
LayoutBuilder.selectCavity()
Returns the select cavity
License requirements: None. |
SelectBodyList |
PiercingInsertBuilder.selectDieInsertForCavity()
Returns the select die insert for cavity.
|
SelectBodyList |
ElectrodeCopyBuilder.selectElectrode()
Returns the selected electrode
License requirements: None. |
SelectBodyList |
ElectrodeCopyBuilder.selectFromFace()
Returns the selected 'from' face
License requirements: None. |
SelectBodyList |
SubInsertBuilder.selectHead()
Returns the head of sub-insert
License requirements: None. |
SelectBodyList |
LayoutRepositionBuilder.selectInstance()
Returns the select instance
License requirements: None. |
SelectBodyList |
CalculateAreaBuilder.selectionTarget()
Returns the target body to calculate area.
|
SelectBodyList |
PiercingInsertBuilder.selectScrap()
Returns the select scraps for pierce insert design.
|
SelectBodyList |
MWDefineSheetsBuilder.selectSheetBodies()
Returns the select sheets is for selecting region, parting and patched sheets to form a new sheet
License requirements: None. |
SelectBodyList |
PocketBuilder.selectTarget()
Returns the target part selection
License requirements: None. |
SelectBodyList |
PiercingInsertBuilder.selectUserDefinedDieInsertForEdit()
Returns the selected user defined die insert to edit.
|
SelectBodyList |
WorkpieceBuilder.selectWorkPieceBody()
Returns the work piece body selection
License requirements: None. |
SelectBodyList |
QuickQuotationBuilder.selSheetBody()
Returns the selected sheet body.
|
SelectBodyList |
ElectrodeCopyBuilder.selToFace()
Returns the selected 'to' face
License requirements: None. |
SelectBodyList |
TrimSolidBuilder.sheetBody()
Returns the sheet body to create trim solid.
|
SelectBodyList |
MWCopySheetsBuilder.sheetsSelection()
Returns the sheets selection for selecting the parting and/or patched sheets to be copied
License requirements: None. |
SelectBodyList |
DieEngStampingOutputBuilder.sourceBody()
Returns the select die engineering sheet bodies
License requirements: die_engineering ("DIE ENGINEERING") . |
SelectBodyList |
ScrapDesignBuilder.splitScrap()
Returns the scrap to be splitted or merged
License requirements: None. |
SelectBodyList |
DieEngStampingCarryoverBuilder.stampingOutput()
Returns the stamping output
License requirements: None. |
SelectBodyList |
TrimMoldComponentsBuilder.targetBodies()
Returns the target bodies which collects the bodies to be trimmed or untrimmed.
|
SelectBodyList |
ChannelAdjustBuilder.targetChannel()
Returns the cooling channel to be adjusted.
|
SelectBodyList |
ElectrodeInitializationBuilder.workpieceList()
Returns the utility to get the workpiece list to create an electrode design project.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.