Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Method and Description |
---|---|
RegionPoint |
Part.createEmptyRegionPoint()
Creates an empty item that contains a point and its corresponding body context for a region
License requirements: None. |
RegionPoint |
Part.createRegionPoint(Point point,
Body body)
Creates an item that contains a point and its corresponding body context for a region
License requirements: None. |
RegionPoint |
RegionPointList.findItem(int index)
Returns the object at the input index.
|
RegionPoint[] |
RegionPointList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
RegionPointList.append(RegionPoint object)
Appends an object to the list
License requirements: None. |
void |
RegionPointList.append(RegionPoint[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
RegionPointList.erase(RegionPoint obj)
Erases the object from the list, but does not delete the object.
|
void |
RegionPointList.erase(RegionPoint obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
RegionPointList.findIndex(RegionPoint obj)
Finds the index where the input object appears.
|
void |
RegionPointList.insert(int location,
RegionPoint object)
Inserts an object at the specified location
License requirements: None. |
void |
RegionPointList.setContents(RegionPoint[] objects)
Sets the contents of the entire list.
|
void |
RegionPointList.swap(RegionPoint object1,
RegionPoint object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.