Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PreviewPropertiesBuilder.PartCreationOptions |
PreviewPropertiesBuilder.PartCreationOptions.ON_DEMAND
Interactive only option that allows the part preview to be created by selecting the Create Now button
|
static PreviewPropertiesBuilder.PartCreationOptions |
PreviewPropertiesBuilder.PartCreationOptions.ON_SAVE
Part preview will be created when the part is saved
|
Modifier and Type | Method and Description |
---|---|
PreviewPropertiesBuilder.PartCreationOptions |
PreviewPropertiesBuilder.partCreation()
Returns the part creation.
|
static PreviewPropertiesBuilder.PartCreationOptions |
PreviewPropertiesBuilder.PartCreationOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PreviewPropertiesBuilder.PartCreationOptions |
PreviewPropertiesBuilder.PartCreationOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PreviewPropertiesBuilder.PartCreationOptions[] |
PreviewPropertiesBuilder.PartCreationOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PreviewPropertiesBuilder.setPartCreation(PreviewPropertiesBuilder.PartCreationOptions partCreation)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.