Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static PlotBuilder.RotationOption |
PlotBuilder.RotationOption.DEGREE0
0 degree rotation
|
static PlotBuilder.RotationOption |
PlotBuilder.RotationOption.DEGREE180
180 degree rotation
|
static PlotBuilder.RotationOption |
PlotBuilder.RotationOption.DEGREE270
270 degree rotation
|
static PlotBuilder.RotationOption |
PlotBuilder.RotationOption.DEGREE90
90 degree rotation
|
Modifier and Type | Method and Description |
---|---|
PlotBuilder.RotationOption |
PlotBuilder.rotation()
Returns the rotation of the banner.
|
static PlotBuilder.RotationOption |
PlotBuilder.RotationOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlotBuilder.RotationOption |
PlotBuilder.RotationOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlotBuilder.RotationOption[] |
PlotBuilder.RotationOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PlotBuilder.setRotation(PlotBuilder.RotationOption rotation)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.