Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.FLAT
The fastest shading method.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.GOURAUD
Provides smooth interpolated colors.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.HYBRID_RADIOSITY
Uses standard rendering techniques to calculate direct lighting
together with radiosity processing for indirect lighting for
image rendering.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.IMPROVED
Shading with textures material parameters highlights and shadows.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.PHONG
Provides smoother highlights than Gouraud shading,
but otherwise supports the same level of functionality.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.PHOTO_REALISTIC
All the features of the Improved method, plus support for
anti-aliasing and transparency.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.PREVIEW
An improvement over the Improved method.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.RADIOSITY
An iterative light processing method where indirect lighting
in a scene is derived from direct light bouncing off of surfaces
before an image is rendered.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.RAY_TRACED
Produces photo-realistic images generated with ray tracing.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.RAY_TRACED_FFA
Same as the Ray Traced option, but with
Feature Following Anti-aliasing.
|
Modifier and Type | Method and Description |
---|---|
ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.method()
Returns the method to use for the generation of the High Quality Image.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelingViewHighQualityImage.ShadeMethod |
ModelingViewHighQualityImage.ShadeMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelingViewHighQualityImage.ShadeMethod[] |
ModelingViewHighQualityImage.ShadeMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ModelingViewHighQualityImage.setMethod(ModelingViewHighQualityImage.ShadeMethod method)
Sets the method to use for the generation of the High Quality Image.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.