Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static ModelingViewHighQualityImage.FormatType |
ModelingViewHighQualityImage.FormatType.QTVR_OBJECT_HIGH
Quick Time Virtual Reality object movie , which is a set of image of an
object in different rotations.
|
static ModelingViewHighQualityImage.FormatType |
ModelingViewHighQualityImage.FormatType.QTVR_OBJECT_LOW
Quick Time Virtual Reality object movie, which is a set of image of an
object in different rotations.
|
static ModelingViewHighQualityImage.FormatType |
ModelingViewHighQualityImage.FormatType.QTVR_PANORAMA
Quick Time Virtual Reality panoramic movie, which is a set of images
from a fixed viewpoint.
|
static ModelingViewHighQualityImage.FormatType |
ModelingViewHighQualityImage.FormatType.RASTER_IMAGE
A normal single raster image
|
Modifier and Type | Method and Description |
---|---|
ModelingViewHighQualityImage.FormatType |
ModelingViewHighQualityImage.format()
Returns the format to use for the generation of the High Quality Image.
|
static ModelingViewHighQualityImage.FormatType |
ModelingViewHighQualityImage.FormatType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelingViewHighQualityImage.FormatType |
ModelingViewHighQualityImage.FormatType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelingViewHighQualityImage.FormatType[] |
ModelingViewHighQualityImage.FormatType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ModelingViewHighQualityImage.setFormat(ModelingViewHighQualityImage.FormatType format)
Sets the format to use for the generation of the High Quality Image.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.