Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.FS_RGB
The pixel conversion process uses the Floyd-Steinberg dither
algorithm to distribute the color error across the picture.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.FS_RGB_PLUS_NOISE
The Floyd-Steinberg algorithm is augmented with the addition
of random noise to the initial RGB values before the dither
takes place.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.GRAY_SCALE
Each pixel is converted to a gray level using the NTSC color
to gray scale conversion.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.MONOCHROME
Pixels are converted to black and white and dithered using
the Floyd-Steinberg algorithm.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.NEAREST_RGB
Conversion is to the nearest RGB value in the color lookup table.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.ORDERED_DITHER
A color dither matrix screens pixel colors.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.RGB_PLUS_NOISE
The RGB algorithm is augmented with the addition of
random noise to the initial RGB values before the
dither takes place.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.TC_PLUS_NOISE
Random noise is added to each pixel where the noise is
specifically tailored for true color display devices.
|
Modifier and Type | Method and Description |
---|---|
ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.displayTechnique()
Returns the display technique to use for the generation of the High Quality Image.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ModelingViewHighQualityImage.DisplayTechniqueType |
ModelingViewHighQualityImage.DisplayTechniqueType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ModelingViewHighQualityImage.DisplayTechniqueType[] |
ModelingViewHighQualityImage.DisplayTechniqueType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ModelingViewHighQualityImage.setDisplayTechnique(ModelingViewHighQualityImage.DisplayTechniqueType displayTechnique)
Sets the display technique to use for the generation of the High Quality Image.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.