Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Interface and Description |
---|---|
interface |
InfiniteLine
Represents a infinite line curve.
|
Modifier and Type | Field and Description |
---|---|
Line |
SelectLine.ValueData.selection
selected object
|
Line |
SelectLine.ValueWithCaeSetObjectInfoData.selection
selected object
|
Line |
SelectLine.ValueWithSnapData.selection1
first selected object
|
Line |
SelectLine.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
Line |
LineCollection.createFaceAxis(IParameterizedSurface face,
SmartObject.UpdateOption updateOption)
Create a Axis line base on a Cylider, Cone, Torus or Revolve face
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Line |
LineCollection.createFaceAxisNoExtension(IParameterizedSurface face,
SmartObject.UpdateOption updateOption)
Create a Axis line base on a Cylider, Cone, Torus or Revolve face.
|
Line |
LineCollection.createFaceAxisNoParentLoadRequired(IParameterizedSurface face,
SmartObject.UpdateOption updateOption)
Create a Axis line base on a Cylider, Cone, Torus or Revolve face.
|
Line |
CurveCollection.createLine(Point3d startPoint,
Point3d endPoint)
Creates a
Line . |
Line |
CurveCollection.createLine(Point startPoint,
Point endPoint)
|
Line |
LineCollection.findObject(String journalIdentifier)
Finds the
Line with the given identifier as recorded in a journal. |
Line |
SelectLine.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
Direction |
DirectionCollection.createDirection(Line line,
Sense sense,
SmartObject.UpdateOption updateOption)
Creates a
nxopen.Direction using a Line . |
InfiniteLine |
CurveCollection.createPairedInfiniteLine(Line line)
Creates a paired
InfiniteLine that is paired to the specified line. |
void |
SelectLine.setValue(Line selection)
Sets the object being selected
License requirements: None. |
void |
SelectLine.setValue(Line selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
void |
SelectLine.setValueWithCaeSetObjectInfo(Line selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
void |
SelectLine.setValueWithSnap(InferSnapType.SnapType snapType,
Line selection1,
View view1,
Point3d point1,
Line selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
Modifier and Type | Method and Description |
---|---|
RelatedNodeMethod |
SmartSelectionManager.createRelatedNodeMethod(Line[] seedTags)
Creates a related node method
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
AssociativeLineBuilder |
BaseFeatureCollection.createAssociativeLineBuilder(Line nonAssociativeLine)
Creates a
AssociativeLineBuilder
License requirements: None. |
Modifier and Type | Interface and Description |
---|---|
interface |
LineSegment
Represents a line segment.
|
Modifier and Type | Method and Description |
---|---|
Line |
RouteSegmentFont.segment()
Returns
License requirements: routing_base ("Routing Basic") . |
Modifier and Type | Method and Description |
---|---|
void |
GapDisplayBuilder.createBuilder(Line selLine,
Line crossLine,
double gapWidth,
Point3d gapStartPoint,
Point3d gapEndPoint,
boolean bridgeOverGap,
boolean arcOrientation)
Takes selected line, gap start and end points, and gap
type settings in to initialise builder data.
|
void |
AddFontBuilder.setBuilderData(Line selLine,
double[] lineCoords,
String fontName,
double fontScale,
int fontLayer)
Takes selected line and information on the font selected which will be used to build the font
License requirements: routing_base ("Routing Basic") . |
void |
GapDisplayBuilder.setBuilderData(Line selLine,
Line crossLine,
double gapWidth,
Point3d gapStartPoint,
Point3d gapEndPoint,
boolean bridgeOverGap,
boolean arcOrientation)
Takes selected line, gap start and end points, and gap
type settings in to set builder data.
|
void |
RouteSegmentFont.setSegment(Line segTag)
Sets
License requirements: routing_base ("Routing Basic") . |
Modifier and Type | Method and Description |
---|---|
Line |
SectionLineCreationBuilder.createTemporaryLine(Point3d pointData,
Vector3d direction)
Create temporary line
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Modifier and Type | Method and Description |
---|---|
void |
SectionLineCreationBuilder.removeAll(Line[] curveList)
Remove all cut segments
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
void |
SectionLineCreationBuilder.removeLast(Line curveTag)
Remove the last cut segment
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.