Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.display |
Provides classes and interfaces for display.
|
Modifier and Type | Field and Description |
---|---|
static LightType |
LightType.AMBIENT
An ambient light provides global illumination
for the scene.
|
static LightType |
LightType.DISTANT
A distant light can be thought of as being
located for all practical purposes infinitely far away,
such as the sun.
|
static LightType |
LightType.EYE
An eye light is Located at the viewpoint or directly
on the Z axis of the screen.
|
LightType |
Light.LightTypeData.lightType
the type of light
|
static LightType |
LightType.POINT
A point light emits light equally in all directions.
|
static LightType |
LightType.SCENE
A scene lights is a light whose parameters, except for
intensity, are fixed.
|
static LightType |
LightType.SPOT
A spot light is the same as a point light,
except that it is constrained by a cone shape.
|
Modifier and Type | Method and Description |
---|---|
static LightType |
LightType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LightType |
LightType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LightType[] |
LightType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
LightType |
LightBuilder.lightType()
Returns the light type for a particular light
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
LightBuilder.setLightType(LightType lightType)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.