Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.SteeringWheelPedalType.CSYS
No steering wheel or pedal, use csys to define
the position and orientation of hand or foot
|
static HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.SteeringWheelPedalType.CURVE
Use curve steering wheel or pedal
|
static HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.SteeringWheelPedalType.SAE
Use sae data to define steering wheel or pedal
|
static HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.SteeringWheelPedalType.SOLID
Use solid steering wheel or pedal
|
Modifier and Type | Method and Description |
---|---|
HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.getHandFootDataType(HumanData.HandFootType handFoot,
HumanData.SideType side)
Get the steering wheel and pedal types of hand foot data
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
static HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.SteeringWheelPedalType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanPosturePredictionBuilder.SteeringWheelPedalType |
HumanPosturePredictionBuilder.SteeringWheelPedalType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanPosturePredictionBuilder.SteeringWheelPedalType[] |
HumanPosturePredictionBuilder.SteeringWheelPedalType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HumanPosturePredictionBuilder.setHandFootDataType(HumanData.HandFootType handFoot,
HumanData.SideType side,
HumanPosturePredictionBuilder.SteeringWheelPedalType steeringWheelPedalType)
Set the steering wheel and pedal types of hand foot data.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.