Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static HumanPosturePredictionBuilder.OccupantType |
HumanPosturePredictionBuilder.OccupantType.DRIVER
Indicate Driver
|
static HumanPosturePredictionBuilder.OccupantType |
HumanPosturePredictionBuilder.OccupantType.FRONT_PASSENGER
Indicate Front passenger
|
static HumanPosturePredictionBuilder.OccupantType |
HumanPosturePredictionBuilder.OccupantType.REAR_PASSENGER
Indicate Rear passenger
|
Modifier and Type | Method and Description |
---|---|
HumanPosturePredictionBuilder.OccupantType |
HumanPosturePredictionBuilder.occupant()
Returns the occupant type: driver, front passenger or rear passenger.
|
static HumanPosturePredictionBuilder.OccupantType |
HumanPosturePredictionBuilder.OccupantType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanPosturePredictionBuilder.OccupantType |
HumanPosturePredictionBuilder.OccupantType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanPosturePredictionBuilder.OccupantType[] |
HumanPosturePredictionBuilder.OccupantType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HumanPosturePredictionBuilder.setOccupant(HumanPosturePredictionBuilder.OccupantType occupantType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.