Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.WeightType |
HumanData.WeightType.CUSTOM
Indicate weight value is the actual weight of the human
|
static HumanData.WeightType |
HumanData.WeightType.PERCENTILE1
Indicate weight is 1% of population
|
static HumanData.WeightType |
HumanData.WeightType.PERCENTILE5
Indicate weight is 5% of population
|
static HumanData.WeightType |
HumanData.WeightType.PERCENTILE50
Indicate weight is 50% of population
|
static HumanData.WeightType |
HumanData.WeightType.PERCENTILE95
Indicate weight is 95% of population
|
static HumanData.WeightType |
HumanData.WeightType.PERCENTILE99
Indicate weight is 99% of population
|
static HumanData.WeightType |
HumanData.WeightType.REGRESS
Indicate weight value is computed
|
Modifier and Type | Method and Description |
---|---|
static HumanData.WeightType |
HumanData.WeightType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.WeightType |
HumanData.WeightType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.WeightType[] |
HumanData.WeightType.values()
Returns an array that contains the values for this enum.
|
HumanData.WeightType |
HumanData.weightOption()
Returns the weight type for weight value
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Modifier and Type | Field and Description |
---|---|
HumanData.WeightType |
HumanBuilder.WeightData.weightType
Flag for percentile weight in database or actual weight value
|
Modifier and Type | Method and Description |
---|---|
void |
HumanBuilder.setWeightData(HumanData.WeightType weightType,
double weight,
HumanData.WeightUnitType weightUnit)
Sets human weight data
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.