Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.StatureType |
HumanData.StatureType.CUSTOM
Indicate stature value is the actual height height of the human
|
static HumanData.StatureType |
HumanData.StatureType.PERCENTILE1
Indicate stature is 1% of population
|
static HumanData.StatureType |
HumanData.StatureType.PERCENTILE5
Indicate stature is 5% of population
|
static HumanData.StatureType |
HumanData.StatureType.PERCENTILE50
Indicate stature is 50% of population
|
static HumanData.StatureType |
HumanData.StatureType.PERCENTILE95
Indicate stature is 95% of population
|
static HumanData.StatureType |
HumanData.StatureType.PERCENTILE99
Indicate stature is 99% of population
|
static HumanData.StatureType |
HumanData.StatureType.REGRESS
Indicate stature value is computed
|
Modifier and Type | Method and Description |
---|---|
HumanData.StatureType |
HumanData.statureOption()
Returns the stature type for stature value
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
static HumanData.StatureType |
HumanData.StatureType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.StatureType |
HumanData.StatureType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.StatureType[] |
HumanData.StatureType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Field and Description |
---|---|
HumanData.StatureType |
HumanBuilder.StatureData.statureType
Flag for percentile stature in database or actual stature measure
|
Modifier and Type | Method and Description |
---|---|
void |
HumanBuilder.setStatureData(HumanData.StatureType statureType,
double stature,
HumanData.StatureUnitType statureUnit)
Sets human stature data
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.