Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.InverseKinematicsType |
HumanData.InverseKinematicsType.ACTIVE_REACH
Indicate active reach type of inverse kinematics
|
static HumanData.InverseKinematicsType |
HumanData.InverseKinematicsType.DYNAMIC_DRAG
Indicate dynamic drag type of inverse kinematics
|
Modifier and Type | Method and Description |
---|---|
static HumanData.InverseKinematicsType |
HumanData.InverseKinematicsType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.InverseKinematicsType |
HumanData.InverseKinematicsType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.InverseKinematicsType[] |
HumanData.InverseKinematicsType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
HumanData.InverseKinematicsType |
HumanBuilder.inverseKinematicsType()
Returns the type of inverse kinematics: dynamic drag or active reach
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Modifier and Type | Method and Description |
---|---|
void |
HumanBuilder.setInverseKinematicsType(HumanData.InverseKinematicsType type)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.