Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.InverseKinematicsHeadEyeType |
HumanData.InverseKinematicsHeadEyeType.FIXATE
Indicate the position of head and eye is fixate
|
static HumanData.InverseKinematicsHeadEyeType |
HumanData.InverseKinematicsHeadEyeType.FOLLOW_LAST_DEFINED
Indicate the position of head and eye follow the last defined position
|
Modifier and Type | Method and Description |
---|---|
static HumanData.InverseKinematicsHeadEyeType |
HumanData.InverseKinematicsHeadEyeType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.InverseKinematicsHeadEyeType |
HumanData.InverseKinematicsHeadEyeType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.InverseKinematicsHeadEyeType[] |
HumanData.InverseKinematicsHeadEyeType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
HumanData.InverseKinematicsHeadEyeType |
HumanBuilder.headEyeType()
Returns the head eye type of active reach
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Modifier and Type | Method and Description |
---|---|
void |
HumanBuilder.setHeadEyeType(HumanData.InverseKinematicsHeadEyeType headEyeType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.