Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.InverseKinematicsBalanceType |
HumanData.InverseKinematicsBalanceType.ALLOW_STEP
Indicate human is allowed to move one step to keep balance
|
static HumanData.InverseKinematicsBalanceType |
HumanData.InverseKinematicsBalanceType.KEEP_SEATED
Indicate human is in a seated position and thus supported by the lower torso
|
static HumanData.InverseKinematicsBalanceType |
HumanData.InverseKinematicsBalanceType.NO_STEP
Indicate human foot is fixate without step
|
Modifier and Type | Method and Description |
---|---|
static HumanData.InverseKinematicsBalanceType |
HumanData.InverseKinematicsBalanceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.InverseKinematicsBalanceType |
HumanData.InverseKinematicsBalanceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.InverseKinematicsBalanceType[] |
HumanData.InverseKinematicsBalanceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
HumanData.InverseKinematicsBalanceType |
HumanBuilder.balanceType()
Returns the balance type of active reach
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Modifier and Type | Method and Description |
---|---|
void |
HumanBuilder.setBalanceType(HumanData.InverseKinematicsBalanceType balanceType)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.