Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.HandGoalType |
HumanData.HandGoalType.GOAL_CSYS
Indicate the hand goal is csys
|
static HumanData.HandGoalType |
HumanData.HandGoalType.GOAL_POINT
Indicate the hand goal is point
|
static HumanData.HandGoalType |
HumanData.HandGoalType.HAND_FIGURE
Indicate the hand goal is hand figure
|
Modifier and Type | Method and Description |
---|---|
static HumanData.HandGoalType |
HumanData.HandGoalType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.HandGoalType |
HumanData.HandGoalType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.HandGoalType[] |
HumanData.HandGoalType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
HumanData.HandGoalType |
HumanBuilder.getHandGoalType(HumanData.SideType side)
Gets hand goal type for active reach
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Modifier and Type | Method and Description |
---|---|
void |
HumanBuilder.setHandGoalType(HumanData.SideType side,
HumanData.HandGoalType goalType)
Sets hand goal type for active reach
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.