Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Interface and Description |
---|---|
interface |
MeasureAngle
Represents a single valued Angle measurement
To create or edit an instance of this class, use MeasureAngleBuilder Created in NX4.0.0 |
interface |
MeasureBodies
Represents the measurement specific mass properties for a set of bodies
To create or edit an instance of this class, use MeasureFaceBuilder Created in NX4.0.0 |
interface |
MeasureDistance
Represents a single valued distance measurement
To create or edit an instance of this class, use MeasureDistanceBuilder Created in NX4.0.0 |
interface |
MeasureFaces
Represents the measurement of perimeter and area of a set of faces
To create or edit an instance of this class, use MeasureFaceBuilder Created in NX4.0.0 |
interface |
MeasureLength
Represents a single valued length measurement .
|
interface |
MeasurePoint
Represents a point measurement .
|
interface |
MeasurePolarAngle
Represents a single valued polar angle measurement .
|
interface |
MeasurePolarArea
Represents a single valued polar area measurement .
|
interface |
MeasurePolarRadius
Represents a single valued polar radius measurement .
|
interface |
MeasureRectangularExtreme
Represents a rectangular extreme point measurement .
|
interface |
SingleMeasure
Represents a single valued measurement .
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.