Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static FollowFilletRuleType |
FollowFilletRuleType.CONNECTED
Connected Curves
|
FollowFilletRuleType |
FollowFilletRule.Data.method
Selection Intent method
|
static FollowFilletRuleType |
FollowFilletRuleType.TANGENT
Tangent Curves
|
Modifier and Type | Method and Description |
---|---|
static FollowFilletRuleType |
FollowFilletRuleType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FollowFilletRuleType |
FollowFilletRuleType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FollowFilletRuleType[] |
FollowFilletRuleType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
FollowFilletRule |
ScRuleFactory.createRuleFollowFillet(nxopen.features.Feature[] features,
Body[] bodies,
ICurve[] basicCurves,
ICurve seedWireframe,
ICurve endWireframe,
boolean isFromSeedStart,
Point3d seedPoint,
double gapTolerance,
double angleTolerance,
FollowFilletRuleType method)
Creates selection intent rule:
FollowFilletRule
License requirements: gateway ("UG GATEWAY") Created in NX4.0.0 |
FollowFilletRule |
ScRuleFactory.createRuleFollowFillet(nxopen.features.Feature[] features,
Body[] bodies,
ICurve[] basicCurves,
ICurve seedWireframe,
Point3d seedPoint,
double gapTolerance,
double angleTolerance,
FollowFilletRuleType method)
Creates selection intent rule:
FollowFilletRule with stop at intersection option ON
License requirements: gateway ("UG GATEWAY") Created in NX7.5.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.