Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
ExpressionCollectorSet |
Part.createEmptyExpressionCollectorSet()
Creates an empty ExpressionCollectorSet item
License requirements: None. |
ExpressionCollectorSet |
Part.createExpressionCollectorSet(ScCollector collector,
String value,
String unitsType,
int index)
Creates an ExpressionCollectorSet item that contains a
ScCollector collection
and a corresponding expression
License requirements: None. |
ExpressionCollectorSet |
ExpressionCollectorSetList.findItem(int index)
Returns the object at the input index.
|
ExpressionCollectorSet[] |
ExpressionCollectorSetList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ExpressionCollectorSetList.append(ExpressionCollectorSet object)
Appends an object to the list
License requirements: None. |
void |
ExpressionCollectorSetList.append(ExpressionCollectorSet[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
ExpressionCollectorSetList.erase(ExpressionCollectorSet obj)
Erases the object from the list, but does not delete the object.
|
void |
ExpressionCollectorSetList.erase(ExpressionCollectorSet obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
ExpressionCollectorSetList.findIndex(ExpressionCollectorSet obj)
Finds the index where the input object appears.
|
void |
ExpressionCollectorSetList.insert(int location,
ExpressionCollectorSet object)
Inserts an object at the specified location
License requirements: None. |
void |
ExpressionCollectorSetList.setContents(ExpressionCollectorSet[] objects)
Sets the contents of the entire list.
|
void |
ExpressionCollectorSetList.swap(ExpressionCollectorSet object1,
ExpressionCollectorSet object2)
Exchanges the position of two objects inside the list.
|
Modifier and Type | Method and Description |
---|---|
ExpressionCollectorSet |
MigratedPanelBuilder.endConditions()
Returns the end conditions
License requirements: nx_sheet_metal ("NX Sheet Metal") . |
Modifier and Type | Interface and Description |
---|---|
interface |
FaceSetOffset
This class represents a face set (collector) offset data.
|
interface |
TwoExpressionsCollectorSet
Represents a two dimension list item builder
To create a new instance of this class, use Part.createEmptyTwoExpressionsCollectorSet() Created in NX8.5.0 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.