Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgImporter.AspectRatioOptions |
DxfdwgImporter.AspectRatioOptions.AUTOMATIC_CALCULATION |
static DxfdwgImporter.AspectRatioOptions |
DxfdwgImporter.AspectRatioOptions.SCALE_ACADWIDTH_FACTOR_WITH_SPECIFIED_VALUE |
static DxfdwgImporter.AspectRatioOptions |
DxfdwgImporter.AspectRatioOptions.USE_SAME_AS_ACADWIDTH_FACTOR |
static DxfdwgImporter.AspectRatioOptions |
DxfdwgImporter.AspectRatioOptions.USE_VALUE_SPECIFIED_IN_MAPPING_FILE |
Modifier and Type | Method and Description |
---|---|
DxfdwgImporter.AspectRatioOptions |
DxfdwgImporter.aspectRatioOption()
Returns the autocad aspect ratio calculation method - this will decide the NX Aspect ratio method to be used.
|
static DxfdwgImporter.AspectRatioOptions |
DxfdwgImporter.AspectRatioOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgImporter.AspectRatioOptions |
DxfdwgImporter.AspectRatioOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgImporter.AspectRatioOptions[] |
DxfdwgImporter.AspectRatioOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgImporter.setAspectRatioOption(DxfdwgImporter.AspectRatioOptions widthFactorMode)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.