Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.OutputToOption |
DxfdwgCreator.OutputToOption.DRAFTING
output to drafting
|
static DxfdwgCreator.OutputToOption |
DxfdwgCreator.OutputToOption.MODELING
output to modeling
|
Modifier and Type | Method and Description |
---|---|
DxfdwgCreator.OutputToOption |
DxfdwgCreator.outputTo()
Returns the output to - where to put data in model world or layout
License requirements: None. |
static DxfdwgCreator.OutputToOption |
DxfdwgCreator.OutputToOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.OutputToOption |
DxfdwgCreator.OutputToOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.OutputToOption[] |
DxfdwgCreator.OutputToOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setOutputTo(DxfdwgCreator.OutputToOption outputTo)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.