Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DxfdwgCreator.ExportSplinesAsOptions |
DxfdwgCreator.ExportSplinesAsOptions.POLYLINE2D
export faces as facets
|
static DxfdwgCreator.ExportSplinesAsOptions |
DxfdwgCreator.ExportSplinesAsOptions.POLYLINE3D
export faces as polyline mesh
|
static DxfdwgCreator.ExportSplinesAsOptions |
DxfdwgCreator.ExportSplinesAsOptions.SPLINE |
Modifier and Type | Method and Description |
---|---|
DxfdwgCreator.ExportSplinesAsOptions |
DxfdwgCreator.exportSplinesAs()
Returns the export Spline as - this will determine if the spline should be exported as spline, 2D ployline or 3D polyline
License requirements: None. |
static DxfdwgCreator.ExportSplinesAsOptions |
DxfdwgCreator.ExportSplinesAsOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DxfdwgCreator.ExportSplinesAsOptions |
DxfdwgCreator.ExportSplinesAsOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DxfdwgCreator.ExportSplinesAsOptions[] |
DxfdwgCreator.ExportSplinesAsOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DxfdwgCreator.setExportSplinesAs(DxfdwgCreator.ExportSplinesAsOptions exportSplinesAs)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.