Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.assemblies |
Provides classes and interfaces for Assemblies.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.display |
Provides classes and interfaces for display.
|
nxopen.drafting |
Provides classes and interfaces for the Drafting.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.facet |
Provides classes and interfaces for Faceted Representations.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.features.subdivision |
Provides classes and interfaces for Manufacturing.
|
nxopen.fields |
Provides classes and interfaces for Fields.
|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
nxopen.geometricanalysis.sectionanalysis |
Provides classes and interfaces for Section Analysis.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
nxopen.layer |
Provides classes and interfaces for layer.
|
nxopen.layout2d |
Provides classes and interfaces for Manufacturing.
|
nxopen.markup |
Provides classes and interfaces for Manufacturing.
|
nxopen.mechatronics |
Provides classes and interfaces for Mechatronics.
|
nxopen.motion |
Provides classes and interfaces for Motion Simulation.
|
nxopen.positioning |
Provides classes and interfaces for Assembly Positioning and Constraints.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
nxopen.userdefinedobjects |
Provides classes and interfaces for User Defined Objects (UDOs).
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Arc
Represents an arc curve.
|
interface |
AutomaticTraceline
Represents an automatic traceline.
|
interface |
Body
Represents a Body
.
|
interface |
CartesianCoordinateSystem
Represents a cartesian coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCoordinateSystem(nxopen.Point3d, nxopen.Matrix3x3, boolean) Created in NX4.0.0 |
interface |
Conic
Represents a conic curve.
|
interface |
CoordinateSystem
Represents a coordinate system
This is an abstract class . |
interface |
Curve
Represents a curve.
|
interface |
CylindricalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCylindricalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
DatumPlane
Represents a datum plane
This object can not be created by KF it's the display objet of the datum plane . |
interface |
Edge
|
interface |
Ellipse
Represents an ellipse curve.
|
interface |
Face
Represents a face .
|
interface |
Hyperbola
Represents a hyperbola curve.
|
interface |
InfiniteLine
Represents a infinite line curve.
|
interface |
Line
Represents a line curve.
|
interface |
Offset
Represents a
Offset . |
interface |
Parabola
Represents a parabola curve.
|
interface |
Plane
Represents an
Plane class. |
interface |
Point
Represents a smart
Point . |
interface |
Polyline
Represents a polyline curve.
|
interface |
ReferenceSet
|
interface |
Scalar
Represents a scalar.
|
interface |
ScCollector
Sc Collector
To create a new instance of this class, use ScCollectorCollection.createCollector() Created in NX4.0.0 |
interface |
Section
Represents a section
Section consists of "chained_entity", a chain or a single entity of edge or curve. |
interface |
Sketch
Represents a sketch
Use the SketchCollection class to create a sketch. |
interface |
SketchAssociativeTrim
Represents a sketch associative trim constraint
Use SketchCollection.createSketchAssociativeTrimBuilder(nxopen.SketchAssociativeTrim) to create an instance of this class. |
interface |
SketchConstraint
Represents a constraint in a sketch.
|
interface |
SketchDimensionalConstraint
Represents a dimensional constraint
To create an instance of this class refer to Sketch Created in NX3.0.0 |
interface |
SketchG1Constraint
Represents a sketch G1 constraint
Use Features.FeatureCollection#createSketchSplineBuilder to create an instance of this class. |
interface |
SketchG2Constraint
Represents a sketch G2 constraint
Use Features.FeatureCollection#createSketchSplineBuilder to create an instance of this class. |
interface |
SketchGeometricConstraint
|
interface |
SketchHelpedDimensionalConstraint
Represents a dimensional sketch constraint that has a help point or help parameter
. |
interface |
SketchHelpedGeometricConstraint
Represents a geometric sketch constraint that has a help point or help parameter
To obtain an instance of this class, use Sketch . |
interface |
SketchOffset
Represents a sketch offset constraint
Use SketchCollection.createSketchOffsetBuilder(nxopen.SketchOffset) to create an instance of this class. |
interface |
SketchPattern
Represents a sketch pattern constraint
Use SketchCollection.createSketchPatternBuilder(nxopen.SketchPattern) to create an instance of this class. |
interface |
SketchTangentConstraint
Represents a tangent constraint
To create an instance of this object use Sketch.createTangentConstraint(nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp, nxopen.Sketch.ConstraintGeometry, nxopen.Sketch.ConstraintGeometryHelp) Created in NX3.0.0 |
interface |
SmartObject
Represents a smart object.
|
interface |
SphericalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createSphericalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
Spline
Represents a spline curve.
|
interface |
SubdivisionMeshBody
Represents a subdivision mesh.
|
interface |
SubdivisionMeshEdge
Represents a subdivision mesh edge.
|
interface |
SubdivisionMeshFace
Represents a subdivision mesh face.
|
interface |
SubdivisionMeshVertex
Represents a subdivision mesh vertex.
|
interface |
Traceline
Represents a traceline.
|
interface |
Xform
Represents a smart xform
To create a new instance of this class, use XformCollection.createXform(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d, nxopen.SmartObject.UpdateOption, double) Created in NX3.0.0 |
Modifier and Type | Field and Description |
---|---|
DisplayableObject |
DisplayManager.J3dData.eid
NX identifier for this shape
|
DisplayableObject |
SectionElementData.SectionElementData1.endConnector
The element that is connected to the
section_element, at the end_point - this can be curve or point
|
DisplayableObject |
SectionElementData.SectionElementData1.sectionElement
The element that constructs the section - this can be curve or point.
|
DisplayableObject |
RegionBoundaryRule.Data.seedObj
Face or Sketch
|
DisplayableObject |
SelectDisplayableObject.ValueData.selection
selected object
|
DisplayableObject |
SelectDisplayableObject.ValueWithCaeSetObjectInfoData.selection
selected object
|
DisplayableObject |
SelectDisplayableObject.ValueWithSnapData.selection1
first selected object
|
DisplayableObject |
SelectDisplayableObject.ValueWithSnapData.selection2
second selected object
|
DisplayableObject |
SectionElementData.SectionElementData1.startConnector
The element that is connected to the
section_element, at the start_point - this can be curve or point
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
View.askVisibleObjects()
Returns an array of objects visible in a view
License requirements: None. |
DisplayableObject |
DatumCollection.findObject(String journalIdentifier)
Finds the datum with the given identifier as recorded in a journal.
|
DisplayableObject |
DatumConstraint.geometry()
Returns
License requirements: solid_modeling ("SOLIDS MODELING") . |
DisplayableObject[] |
SelectDisplayableObjectList.getArray()
Returns the list of objects in the selection list.
|
DisplayableObject[] |
CutView.getCutBodies()
Find the cut bodies in a cut view.
|
DisplayableObject[] |
CutViewCollection.getCutViewsOfObject(Body body)
Find the cut views of an object.
|
DisplayableObject |
SelectDisplayableObject.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
boolean |
SelectDisplayableObjectList.add(DisplayableObject object)
Adds an object to the list
License requirements: None. |
boolean |
SelectDisplayableObjectList.add(DisplayableObject[] objects)
Adds a set of objects to the list
License requirements: None. |
boolean |
SelectDisplayableObjectList.add(DisplayableObject selection,
View view,
Point3d point)
Adds the object with the objects view and objects point
License requirements: None. |
void |
DraftingManager.addCutObject(DisplayableObject object)
Identify object to be drawn as Cut in Drafting
License requirements: None. |
void |
Sketch.addGeometry(DisplayableObject crv)
Adds a curve or point to the sketch.
|
void |
Sketch.addGeometry(DisplayableObject crv,
Sketch.InferConstraintsOption inferCoincidentConstraints)
Adds a curve or point to the sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
DisplayModification.apply(DisplayableObject[] objects)
Apply this display modification to a set of objects
License requirements: None. |
void |
ViewDependentDisplayManager.applySegmentEdit(DisplayableObject object,
NXColor color,
ViewDependentDisplayManager.Font font,
ViewDependentDisplayManager.Width width,
double[] segmentStart,
double[] segmentEnd)
Applies a wireframe edit to specified objects in a view.
|
void |
ViewDependentDisplayManager.applySegmentEdit(DisplayableObject object,
ViewDependentDisplayManager.Font font,
ViewDependentDisplayManager.Width width,
double[] segmentStart,
double[] segmentEnd)
Applies a wireframe edit to specified objects in a view
when the color is the original color
License requirements: None. |
void |
ViewDependentDisplayManager.applyShadeEdit(NXColor shadeColor,
ViewDependentDisplayManager.PartialShading partialShading,
ViewDependentDisplayManager.Translucency translucencyOption,
int translucencyScale,
DisplayableObject[] objects)
Applies a shading edit to specified faces and/or bodies in a view.
|
void |
ViewDependentDisplayManager.applyShadeEdit(ViewDependentDisplayManager.PartialShading partialShading,
ViewDependentDisplayManager.Translucency translucencyOption,
int translucencyScale,
DisplayableObject[] objects)
Applies a shading edit to specified faces and/or bodies in a view when
shade color is original color
License requirements: None. |
void |
ViewDependentDisplayManager.applyWireframeEdit(NXColor color,
ViewDependentDisplayManager.Font font,
ViewDependentDisplayManager.Width width,
DisplayableObject[] objects)
Applies a wireframe edit to specified objects in a view.
|
void |
ViewDependentDisplayManager.applyWireframeEdit(ViewDependentDisplayManager.Font font,
ViewDependentDisplayManager.Width width,
DisplayableObject[] objects)
Applies a wireframe edit to specified objects in a view
when the color is the original color
License requirements: None. |
void |
DisplayManager.blankObjects(DisplayableObject[] objects)
Blank a set of displayable objects.
|
boolean |
SelectDisplayableObjectList.contains(DisplayableObject object)
Returns whether the specified object is already in the list or not.
|
Sketch.CopyObjectData[] |
Sketch.copyObjectsWithTracking(DisplayableObject[] inputObjects)
Creates copies of input objects and constraints between these objects.
|
BodyFeatureRule |
ScRuleFactory.createRuleBodyFeature(nxopen.features.Feature[] features,
boolean includeSheetBodies,
DisplayableObject partOccurrence)
Creates selection intent rule:
BodyFeatureRule for the given feature from a part occurrence, with the option to include or exclude sheet bodies
License requirements: gateway ("UG GATEWAY") . |
BodyFeatureRule |
ScRuleFactory.createRuleBodyFeature(nxopen.features.Feature[] features,
DisplayableObject partOccurrence)
Creates selection intent rule:
BodyFeatureRule for the given feature from a part occurrence. |
CurveFeatureRule |
ScRuleFactory.createRuleCurveFeature(nxopen.features.Feature[] features,
DisplayableObject partOccurrence)
Creates selection intent rule:
CurveFeatureRule for the given feature from a part occurrence. |
EdgeFeatureRule |
ScRuleFactory.createRuleEdgeFeature(nxopen.features.Feature[] features,
DisplayableObject partOccurrence)
Creates selection intent rule:
EdgeFeatureRule for the given feature from a part occurrence. |
FaceFeatureRule |
ScRuleFactory.createRuleFaceFeature(nxopen.features.Feature[] features,
DisplayableObject partOccurrence)
Creates selection intent rule:
FaceFeatureRule for the given feature from a part occurrence. |
FeaturePointsRule |
ScRuleFactory.createRuleFeaturePoints(nxopen.features.Feature[] features,
DisplayableObject partOccurrence)
Creates selection intent rule:
FeaturePointsRule for the given feature from a part occurrence. |
RegionBoundaryRule |
ScRuleFactory.createRuleRegionBoundary(DisplayableObject seedObj,
ICurve[] curves,
Point3d seedPoint,
double distanceTolerance)
Creates selection intent rule:
RegionBoundaryRule
License requirements: gateway ("UG GATEWAY") Created in NX6.0.0 |
Xform |
XformCollection.createXform(DisplayableObject plane,
Direction axis,
SmartObject.UpdateOption updateOption,
double scale)
Creates a Xform based on a plane and a vector.
|
Xform |
XformCollection.createXform(DisplayableObject plane1,
DisplayableObject plane2,
DisplayableObject plane3,
SmartObject.UpdateOption updateOption,
double scale)
Creates a Xform by three planes.
|
Xform |
XformCollection.createXformByPlaneXDirPoint(DisplayableObject plane,
Direction xDirection,
Point point,
SmartObject.UpdateOption updateOption,
double scale,
boolean flipXDirection,
boolean flipZDirection)
Creates a Xform based on a planar face or datum plane, a X-axis vector direction, and a point.
|
void |
Measurement.displayArcLength(DisplayableObject[] selectedObjects)
Calculates and displays 'Total Arc Length' of all the selected objects.
|
Measurement.DisplayMinimumDistanceData |
Measurement.displayMinimumDistance(DisplayableObject object1,
DisplayableObject object2)
Calculates and displays 'Minimum Distance " between objects.
|
void |
MeasureManager.editAngle(Measure feature,
DisplayableObject object1,
MeasureManager.EndpointType qualifier1,
DisplayableObject object2,
MeasureManager.EndpointType qualifier2,
boolean minorAngle)
Edit an angle measurement between two objects.
|
void |
MeasureManager.editAngle(Measure feature,
DisplayableObject object1,
MeasureManager.EndpointType qualifier1,
DisplayableObject object2,
MeasureManager.EndpointType qualifier2,
boolean minorAngle,
boolean trueAngle)
Edit an angle measurement between two objects.
|
void |
MeasureManager.editAngle(String name,
DisplayableObject object1,
MeasureManager.EndpointType qualifier1,
DisplayableObject object2,
MeasureManager.EndpointType qualifier2,
boolean minorAngle)
Edit an embedded angle measurement between two objects.
|
void |
MeasureManager.editAngle(String name,
DisplayableObject object1,
MeasureManager.EndpointType qualifier1,
DisplayableObject object2,
MeasureManager.EndpointType qualifier2,
boolean minorAngle,
boolean trueAngle)
Edit an embedded angle measurement between two objects.
|
void |
MeasureManager.editDistance(Measure feature,
DisplayableObject object1)
Edit a radial distance measure for arcs and circles.
|
void |
MeasureManager.editDistance(Measure feature,
DisplayableObject object1,
DisplayableObject object2,
Direction direction)
Edit a projected minimum distance measure between two objects.
|
void |
MeasureManager.editDistance(Measure feature,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType)
Edit a projected minimum distance measure or clearance distance between two objects.Note that for design in
context the direction vector needs to be in the coordinates of the work part.
|
void |
MeasureManager.editDistance(Measure feature,
DisplayableObject object1,
Point3d startPointForObject1,
DisplayableObject object2,
Point3d startPointForObject2)
Edit a local minimum distance measure between two objects with two start points.
|
void |
MeasureManager.editDistance(String name,
DisplayableObject object1)
Edit an embedded radial distance measure between two objects.
|
void |
MeasureManager.editDistance(String name,
DisplayableObject object1,
DisplayableObject object2)
Edit an embedded minimum or maximum distance measure between two objects.
|
void |
MeasureManager.editDistance(String name,
DisplayableObject object1,
DisplayableObject object2,
Direction direction)
Edit an embedded projected minimum distance measure between two objects.
|
void |
MeasureManager.editDistance(String name,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType)
Edit an embedded projected minimum or clearance distance measure between two objects.
|
void |
MeasureManager.editDistance(String name,
DisplayableObject object1,
Point3d startPointForObject1,
DisplayableObject object2,
Point3d startPointForObject2)
Edit an embedded local minimum distance measure between two objects with two start points.
|
void |
MeasureManager.editLength(Measure feature,
DisplayableObject[] objects)
Edit a length measure.
|
void |
MeasureManager.editLength(String name,
DisplayableObject[] objects)
Edit an embedded length measure.
|
void |
ViewDependentDisplayManager.erase(DisplayableObject[] objects)
Erases specified objects in a view.
|
double |
Measurement.getArcLength(DisplayableObject[] selectedObjects)
Calculates and returns 'Total Arc Length' of all the selected objects.
|
DisplayManager.J3dGeometryData |
DisplayManager.getJ3dGeometry(DisplayableObject eid,
double tolerance,
boolean wireframe)
Returns polygon/vector information for an entity
License requirements: None. |
void |
Sketch.hideDimensions(DisplayableObject[] inputObjects)
Blanks dimensions in the active sketch associated with the input sketch geometry.
|
boolean |
DraftingManager.isCutObject(DisplayableObject object)
Is this object to be drawn as Cut?
|
SmartObject[] |
Sketch.mirrorObjects(DisplayableObject centerline,
SmartObject[] objectsToMirror)
Deprecated.
Deprecated in NX5.0.0. Please use
SketchMirrorBuilder instead.
|
void |
ViewDependentDisplayManager.moveToModel(DisplayableObject[] objects)
Moves view objects to model.
|
void |
ViewDependentDisplayManager.moveToView(DisplayableObject[] objects)
Moves model objects to view.
|
MeasureAngle |
MeasureManager.newAngle(Unit units,
DisplayableObject object1,
MeasureManager.EndpointType qualifier1,
DisplayableObject object2,
MeasureManager.EndpointType qualifier2,
boolean minorAngle)
Create an angle measurement between two objects.
|
MeasureAngle |
MeasureManager.newAngle(Unit units,
DisplayableObject object1,
MeasureManager.EndpointType qualifier1,
DisplayableObject object2,
MeasureManager.EndpointType qualifier2,
boolean minorAngle,
boolean trueAngle)
Create an angle measurement between two objects.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
boolean createGeometry,
DisplayableObject object1,
Point3d startPointForObject1,
DisplayableObject object2,
Point3d startPointForObject2)
Create a local minimum distance measure between two objects with start points
and the option to create smart geoemtry
Features.SewBuilder.Types of allowed input objects include - Point, Curve, Edge, Face, Body, Datum Plane, Datum Axis, Facet Body. |
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1)
Create a radial distance measure for an arc or circle.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1,
DisplayableObject object2,
Direction direction)
Create a projected minimum distance measure between two objects.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType)
Create a projected, minimum clearance or maximum clearance distance measure between two objects.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1,
DisplayableObject object2,
Direction direction,
MeasureManager.ProjectionType projType,
boolean createGeometry)
Create a projected, minimum clearance or maximum clearance distance measure between two objects with the
option to create smart geometry.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1,
MeasureManager.RadialMeasureType mType)
Create a radial/diameter distance measure for an arc or circle.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
DisplayableObject object1,
Point3d startPointForObject1,
DisplayableObject object2,
Point3d startPointForObject2)
Create a local minimum distance measure between two objects with start points.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
MeasureManager.MeasureType minMaxFlag,
boolean createGeometry,
DisplayableObject object1,
DisplayableObject object2)
Create a minimum or maximum distance measure between two objects with the option to create smart geometry.
|
MeasureDistance |
MeasureManager.newDistance(Unit units,
MeasureManager.MeasureType minMaxFlag,
DisplayableObject object1,
DisplayableObject object2)
Create a minimum or maximum distance measure between two objects.
|
MeasureLength |
MeasureManager.newLength(Unit units,
DisplayableObject[] objects)
Creates a arc length object for all the selected objects.
|
boolean |
SelectDisplayableObjectList.remove(DisplayableObject object)
Remove specified object from list.
|
boolean |
SelectDisplayableObjectList.remove(DisplayableObject object,
View view)
Remove specified object from list.
|
boolean |
SelectDisplayableObjectList.remove(InferSnapType.SnapType snapType,
DisplayableObject selection1,
View view1,
Point3d point1,
DisplayableObject selection2,
View view2,
Point3d point2)
Remove specified object from list.
|
boolean |
SelectDisplayableObjectList.removeArray(DisplayableObject[] objects)
Remove specified objects from list.
|
void |
ViewDependentDisplayManager.removeEdit(DisplayableObject[] objects)
Removes edits from specified objects in a view.
|
void |
ViewDependentDisplayManager.removeErasure(DisplayableObject[] objects)
Removes erasures from specified objects in a view.
|
void |
ScCollector.replaceRules(SelectionIntentRule[] rules,
DisplayableObject[] negatedEntities,
boolean createRulesWoUpdate)
Replace collector rules and specify negated entities.
|
void |
SelectDisplayableObjectList.setArray(DisplayableObject[] objects)
Sets the list of objects in the selection list.
|
void |
ViewDependentDisplayManager.setBackground(DisplayableObject[] objects)
Sets visibility of background objects.
|
void |
DatumConstraint.setGeometry(DisplayableObject geometry)
Sets
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
SelectDisplayableObject.setValue(DisplayableObject selection)
Sets the object being selected
License requirements: None. |
void |
SelectDisplayableObject.setValue(DisplayableObject selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
boolean |
SelectDisplayableObjectList.setValueWithCaeSetObjectInfo(DisplayableObject selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObjectList.add(nxopen.TaggedObject) .
|
void |
SelectDisplayableObject.setValueWithCaeSetObjectInfo(DisplayableObject selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
boolean |
SelectDisplayableObjectList.setValueWithSnap(InferSnapType.SnapType snapType,
DisplayableObject selection1,
View view1,
Point3d point1,
DisplayableObject selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
void |
SelectDisplayableObject.setValueWithSnap(InferSnapType.SnapType snapType,
DisplayableObject selection1,
View view1,
Point3d point1,
DisplayableObject selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
void |
DisplayManager.showAdjacent(DisplayableObject[] objects)
|
void |
Sketch.showDimensions(DisplayableObject[] inputObjects)
Unblanks dimensions in the active sketch associated with the input sketch geometry
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
DisplayManager.showObjects(DisplayableObject[] objects,
DisplayManager.LayerSetting layerSetting)
Unblank a set of displayable objects considering the following layer settings if the objects are in invisible layers.
|
void |
DisplayManager.showOnly(DisplayableObject[] objects)
Show a set of displayable objects.
|
void |
DisplayManager.unblankObjects(DisplayableObject[] objects)
Unblank a set of displayable objects.
|
Constructor and Description |
---|
J3dData(DisplayableObject eidInitial,
boolean hasTransformInitial,
boolean sheetInitial,
String nameInitial,
DisplayManager.J3dMaterial materialInitial)
Constructor for the J3dData object.
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
ComponentData.getEntities()
Returns the entities that display the annotation.
|
DisplayableObject[] |
AssociatedObject.getObjects()
Returns the objects.
|
DisplayableObject[] |
LineWeldData.getSideSeamObjects()
Returns the side seam objects.
|
DisplayableObject[] |
LineWeldData.getTopSeamObjects()
Returns the top seam objects.
|
Modifier and Type | Method and Description |
---|---|
TitleBlockCellBuilder |
TitleBlockCollection.createCellBuilder(DisplayableObject object,
boolean isLocked,
int contentType,
String value,
String label,
boolean canLockStatusChange)
Creates a cell builder
License requirements: None. |
EditLeaderBuilder |
AnnotationManager.createEditLeaderBuilder(DisplayableObject tableTag)
|
int |
AssociatedObject.getObjectIndex(DisplayableObject object)
Returns the associated object index
License requirements: None. |
void |
TableEditSettingsBuilder.inheritSettingsFromSelectedObjects(DisplayableObject selectedObject)
Inherit Settings From Selected Objects
License requirements: drafting ("DRAFTING") . |
void |
StyleBuilder.inheritSettingsFromSelectedObjects(DisplayableObject selectedObject)
Inherit Settings From Selected Objects
License requirements: drafting ("DRAFTING") . |
void |
EditSettingsBuilder.inheritSettingsFromSelectedObjects(DisplayableObject selectedObject)
Inherit Settings From Selected Objects
License requirements: drafting ("DRAFTING") . |
Annotation[] |
AnnotationManager.queryPmiFromGeometry(DisplayableObject[] geom)
Finds all PMI symbols that reference the given geometry as an
associated object.
|
void |
MasterCustomSymbolData.setGeometry(DisplayableObject[] geom)
Deprecated.
Deprecated in NX9.0.0. Use
MasterSymbolBuilder instead.
|
void |
AssociatedObject.setObjects(DisplayableObject[] objects)
Sets the objects.
|
void |
LineWeldData.setSideSeamObjects(DisplayableObject[] objects)
Sets the side seam objects.
|
void |
LineWeldData.setTopSeamObjects(DisplayableObject[] objects)
Sets the top seam objects.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Component
Represents a component in a
ComponentAssembly . |
interface |
ExplodedComponent
Represents a
Component within an explosion. |
Modifier and Type | Field and Description |
---|---|
DisplayableObject[] |
ClearanceSet.InterferenceData.interfbodies
the list of interference bodies
|
DisplayableObject |
ClearanceSet.NextInterferenceData.nextobject1
the first object in the pair of the next interference
|
DisplayableObject |
ClearanceSet.NextInterferenceData.nextobject2
the second object in the pair of the next interference
|
Modifier and Type | Method and Description |
---|---|
void |
ClearanceAnalysisBuilder.addException(boolean isExclude,
DisplayableObject comp1,
DisplayableObject comp2,
String text)
Add an exception.
|
void |
ClearanceAnalysisBuilder.addObjectClearanceZone(DisplayableObject object,
Expression expression)
Add a Clearance Zone around an object.
|
void |
ClearanceAnalysisBuilder.addPairClearanceZone(DisplayableObject object1,
DisplayableObject object2,
Expression expression)
Add a Clearance Zone between a pair of objects.
|
void |
ClearanceSet.calculatePenetrationDepth(DisplayableObject[] firstObjects,
DisplayableObject[] secondObjects)
Calculate penetration depth for a set of hard interferences.
|
void |
ClearanceSet.calculatePenetrationDepth(DisplayableObject[] firstObjects,
DisplayableObject[] secondObjects)
Calculate penetration depth for a set of hard interferences.
|
void |
ClearanceSet.createInterferenceGeometry(DisplayableObject[] firstObjects,
DisplayableObject[] secondObjects)
Construct interference geometry for a set of hard interferences.
|
void |
ClearanceSet.createInterferenceGeometry(DisplayableObject[] firstObjects,
DisplayableObject[] secondObjects)
Construct interference geometry for a set of hard interferences.
|
void |
ClearanceAnalysisBuilder.deleteException(DisplayableObject comp1,
DisplayableObject comp2)
Delete an exception.
|
void |
ClearanceSet.deleteInterference(DisplayableObject object1,
DisplayableObject object2)
Deletes the interference for a given object pair.
|
void |
ClearanceAnalysisBuilder.deleteObjectClearanceZone(DisplayableObject object)
Delete an existing Clearance Zone from around an object.
|
void |
ClearanceAnalysisBuilder.deletePairClearanceZone(DisplayableObject object1,
DisplayableObject object2)
Delete an existing Clearance Zone between the given pair of objects.
|
ClearanceSet.InterferenceData |
ClearanceSet.getInterferenceData(DisplayableObject object1,
DisplayableObject object2)
Inquires the data associated with a given pair of interfering objects.
|
boolean |
ClearanceSet.getIsPairChanged(DisplayableObject object1,
DisplayableObject object2)
Inquires if an object pair has changed since the last analysis run.
|
ClearanceAnalysisBuilder.IsPairIncludedData |
ClearanceAnalysisBuilder.getIsPairIncluded(DisplayableObject object1,
DisplayableObject object2)
Inquires if an object pair is to be included in the analysis.
|
ClearanceSet.NextInterferenceData |
ClearanceSet.getNextInterference(DisplayableObject object1,
DisplayableObject object2)
Cycles the interference in a clearance analysis data set.
|
ClearanceAnalysisBuilder.PairClearanceZoneData |
ClearanceAnalysisBuilder.getObjectClearanceZone(DisplayableObject object)
Inquire the Clearance Zone assigned to a given object.
|
ClearanceAnalysisBuilder.PairClearanceZoneData |
ClearanceAnalysisBuilder.getPairClearanceZone(DisplayableObject object1,
DisplayableObject object2)
Inquire the Clearance Zone for a specific pair of objects.
|
void |
ClearanceSet.reanalyzePairs(DisplayableObject[] firstObjects,
DisplayableObject[] secondObjects,
ClearanceSet.ReanalyzePairCalculationMethod calculationMethod)
Reanalyze a set of interferences using the specified analysis method.
|
void |
ClearanceSet.reanalyzePairs(DisplayableObject[] firstObjects,
DisplayableObject[] secondObjects,
ClearanceSet.ReanalyzePairCalculationMethod calculationMethod)
Reanalyze a set of interferences using the specified analysis method.
|
void |
ClearanceSet.setInterferenceText(DisplayableObject object1,
DisplayableObject object2,
String text)
Associates a text string to an interfering object pair.
|
Modifier and Type | Interface and Description | ||
---|---|---|---|
interface |
CAEBody
Represents a CAE body geometry
.
|
||
interface |
CaeDOFSet
Represents a dofset class
CaeDOFSet . |
||
interface |
CAEEdge
Represents a CAE edge geometry
.
|
||
interface |
CAEFace
Represents a CAE face geometry
.
|
||
interface |
CAEVertex
Represents a CAE vertex geometry
.
|
||
interface |
DependentMesh
Represents Mesh Recipe
To create or edit an instance of this class, use DependentMeshBuilder Created in NX5.0.0 |
||
interface |
EdgeDensity
Represents a CAE edge density
.
|
||
interface |
FaceDensity
Represents a CAE face density
.
|
||
interface |
MappedHole
Represents a CAE mapped hole
.
|
||
interface |
MappedMesh
Represents Mesh Recipe
To create or edit an instance of this class, use MappedMeshBuilder Created in NX5.0.0 |
||
interface |
Mesh
Represents a Mesh
For more information, refer to the Solver language documentation
in the
interface Mesh0d
Represents 0d Mesh
To create or edit an instance of this class, use Mesh0dBuilder Created in NX6.0.0 | ||
interface |
Mesh1d
Represents 1d Mesh
To create or edit an instance of this class, use Mesh1dBuilder Created in NX6.0.0 |
||
interface |
Mesh2d
Represents 2d Mesh
This is an abstract class . |
||
interface |
Mesh2dFree
Represents 2d Mesh
To create or edit an instance of this class, use Mesh2dBuilder Created in NX6.0.0 |
||
interface |
Mesh3d
Represents 3d Mesh
To create or edit an instance of this class, use Mesh3dTetBuilder Created in NX6.0.0 |
||
interface |
MeshControl
Represents a MeshControl
To create or edit an instance of this class, use MeshControlBuilder Created in NX5.0.0 |
||
interface |
MeshFollower
Represents Mesh Recipe
This is an abstract class . |
||
interface |
MeshMate
Represents a Mesh Mate
.
|
||
interface |
MeshPoint
Represents a smart
MeshPoint . |
||
interface |
MeshShellFromSolid
Represents 2d Mesh that follows 3d mesh
To create or edit an instance of this class, use SurfaceCoatBuilder Created in NX7.5.0 |
||
interface |
PrimitiveMesh
Represents Primitive Mesh
To create or edit an instance of this class, use PrimitiveMeshBuilder Created in NX7.5.0 |
||
interface |
ResultProbe
Result Probe Object.
|
||
interface |
SimBC
Represents BC class which is a superclass to
SimLoad and SimConstraint . |
||
interface |
SimConstraint
Represents a constraint
To create a new instance of this class, use SimConstraintCollection.createConstraint(java.lang.String, java.lang.String) Created in NX4.0.0 |
||
interface |
SimLoad
Represents a load
To create a new instance of this class, use SimLoadCollection.createLoad(java.lang.String, java.lang.String) Created in NX4.0.0 |
||
interface |
SimSimulationObject
Represents a simulation object
For more information, refer to the Solver language documentation
in the
interface SweptMesh
Represents swept Mesh
To create or edit an instance of this class, use Mesh3dHexBuilder Created in NX6.0.0 | ||
interface |
WeldRow
Represents a CAE weld row
.
|
Modifier and Type | Method and Description |
---|---|
void |
ResultMeasureModelSubsetGeom.setEntities(DisplayableObject[] entities)
Set the geometry entities
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
DAOObjective.getGeometry()
Gets the target geometry
License requirements: None. |
DisplayableObject[] |
DAOConstraintBuilder.getGeometry()
Gets the target geometry
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DAOObjective.setGeometry(DisplayableObject[] geometry)
Sets the target geometry
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
DAOConstraintBuilder.setGeometry(DisplayableObject[] geometry)
Sets the target geometry
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
Modifier and Type | Interface and Description |
---|---|
interface |
Sensor
Represents a
Sensor
To create or edit an instance of this class, use SensorBuilder Created in NX5.0.0 |
interface |
StrainGage
Represents a
StrainGage
To create or edit an instance of this class, use StrainGageBuilder Created in NX6.0.0 |
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
FeatureTeaching.getFaces()
Gets the selected faces
License requirements: fbm_author ("FBM Author") . |
DisplayableObject[] |
FeatureRecognitionBuilder.getSearchGeometry()
Returns the geometry search
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
GeometrySet |
Geometry.appendGeometrySet(GeometrySet templateSet,
DisplayableObject[] entities)
Append an geometry set with dumb rules
License requirements: cam_base ("CAM BASE") . |
void |
FeatureTeaching.setFaces(DisplayableObject[] aFaces)
Sets the selected faces
License requirements: fbm_author ("FBM Author") . |
void |
FeatureRecognitionBuilder.setSearchGeometry(DisplayableObject[] objects)
Sets the geometry to search
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
TrimTaskBuilder.getAssociativeObjects()
Gets the associative objects of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
DisplayableObject[] |
PierceTaskBuilder.getAssociativeObjects()
Gets the associative objects of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
DisplayableObject[] |
FlangeTaskBuilder.getAssociativeObjects()
Gets the associative objects of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Method and Description |
---|---|
void |
TrimTaskBuilder.setAssociativeObjects(DisplayableObject[] objects)
Sets the associative objects of the trim task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
PierceTaskBuilder.setAssociativeObjects(DisplayableObject[] objects)
Sets the associative objects of the pierce task
License requirements: die_engineering ("DIE ENGINEERING") . |
void |
FlangeTaskBuilder.setAssociativeObjects(DisplayableObject[] objects)
Sets the associative objects of the flange task
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Interface and Description |
---|---|
interface |
BoundedGrid
Represents a bounded grid
Bounded grids are not supported in KF. |
interface |
DatumPlaneGrid
Represents a grid on a datum plane
Datum plane grids are not supported in KF. |
interface |
EntitySelectionPlane
Represents a grid on a datum plane
Entity selection planes are not supported in KF. |
interface |
Grid
Represents a grid
Grids are not supported in KF. |
interface |
ImageBase
Represents a
ImageBase that provides
definition, orientation, sizing, and display setting controls for image
based objects. |
interface |
PlanarShipGrid
Represents a planar ship grid.
|
interface |
PlaneGrid
Represents a grid on a bounded plane
Plane grids are not supported in KF. |
interface |
RasterImage
Represents a
RasterImage that provides
placing an imported image onto a plane (with controls for orientation,
sizing, and display) to use as a reference in the model to create geometry. |
Modifier and Type | Method and Description |
---|---|
void |
TransientText.displayTemporaryAbsoluteGeometry(int fontIndex,
View view,
TransientText.ViewType viewType,
DisplayableObject object,
Point3d position)
Displays text as temporary display using absolute geometry.
|
void |
TransientText.displayTemporaryAbsRotScreenSizeGeometry(int fontIndex,
View view,
TransientText.ViewType viewType,
DisplayableObject object,
Point3d position)
Displays text as temporary display using screen geometry but with rotation
defined in absolute space.
|
void |
TransientText.displayTemporaryScreenGeometry(int fontIndex,
View view,
TransientText.ViewType viewType,
DisplayableObject object,
Point3d position)
Displays text as temporary display using screen geometry.
|
Modifier and Type | Method and Description |
---|---|
EditSettingsBuilder |
SettingsManager.createAnnotationEditSettingsBuilder(DisplayableObject[] objects)
Creates a
EditSettingsBuilder
For multiple object settings, first create primary settings builder by passing all selected 'n' objects.Then create 'n-1' secondary builders by passing single selected object starting from second selected object. |
EditViewLabelSettingsBuilder |
SettingsManager.createDrawingEditViewLabelSettingsBuilder(DisplayableObject[] viewLabels)
Creates a
EditViewLabelSettingsBuilder
For multiple object settings, first create primary settings builder by passing all selected 'n' objects.Then create 'n-1' secondary builders by passing single selected object starting from second selected object. |
TableEditSettingsBuilder |
SettingsManager.createTableEditSettingsBuilder(DisplayableObject[] objects)
Creates a
TableEditSettingsBuilder
For multiple object settings, first create primary settings builder by passing all selected 'n' objects.Then create 'n-1' secondary builders by passing single selected object starting from second selected object. |
Modifier and Type | Interface and Description |
---|---|
interface |
BaseHalfSectionLine
Represents a Base Half Section Line.
|
interface |
BasePointToPointSectionLine
Represents a Base Point to Point Section Line.
|
interface |
BaseSteppedSectionLine
Represents a Base Stepped Section Line.
|
interface |
DraftingBody
Represents a drafting body.
|
interface |
DraftingCurve
Represents a Drafting VD Curve.
|
interface |
DrawingRegion
Represents a Drawing Region
To create or edit an instance of this class, use DrawingRegionBuilder Created in NX8.0.0 |
interface |
HalfPictorialSectionLine
Half Pictorial Section Line is used to create a pictorial view with
half of the part sectioned and the other half un-sectioned.
|
interface |
HalfSectionLine
Half Section Line is used to create a view with half of the part
sectioned and the other half un-sectioned.
|
interface |
OrientedSectionLine
Represents a Oriented Section Line.
|
interface |
PictorialSectionLine
A Pictorial Simple or Pictorial Stepped Section Line.
|
interface |
PointAndAngleSectionLine
Point and Angle Section Line lets you create a view with multiple
segment cuts with no bends.
|
interface |
PointToPointSectionLine
Point to Point Section Line lets you create a view with multiple
segment cuts with no bends.
|
interface |
RevolvedSectionLine
Revolved Section Line is used to create section views which are
revolved about an axis.
|
interface |
SectionLine
Represents a Section Line.
|
interface |
SketchedHalfSectionLine
Sketched Half Section Line is sketch based section line.
|
interface |
SketchedPointToPointSectionLine
Sketched Point to Point Section Line is sketch based section line.
|
interface |
SketchedSteppedSectionLine
A Sketched Simple or Stepped Section Line is sketch based section line.
|
interface |
SteppedSectionLine
A Simple or Stepped Section Line.
|
Modifier and Type | Field and Description |
---|---|
DisplayableObject[] |
ViewBreak.ViewBreakDisplayableObjectsAndOffsetsData.displayObjects |
Modifier and Type | Interface and Description |
---|---|
interface |
FacetedBody
Represents a faceted body.
|
interface |
FacetedEdge
Represents a faceted edge.
|
interface |
FacetedFace
Represents a faceted face.
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject |
FillHoleBuilder.fillHoles(boolean globalUpdate)
Fills targeted holes.
|
DisplayableObject[] |
FillHoleBuilder.getAllHoles()
Gets a list of all holes (represented by polylines).
|
DisplayableObject |
FillHoleBuilder.getHoleFillsOnly()
Builds a facet body that contains only the facets of the filled holes.
|
DisplayableObject[] |
FillHoleBuilder.getTargetHolesByEdgeNumber(int numMaxEdges)
Gets a list of targeted holes (represented by polylines) based on number of edges.
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
MasterCutBuilder.getTargetComponents()
The target components that are cut
License requirements: solid_modeling ("SOLIDS MODELING") . |
DisplayableObject |
BooleanBuilder.tool()
Deprecated.
Deprecated in NX5.0.2. Use
Features.BooleanBuilder#toolBodyCollector instead.
|
Modifier and Type | Method and Description |
---|---|
void |
EditDimensionBuilder.attachToNewGeometry(nxopen.annotations.Annotation dimTag,
DisplayableObject newGeometry)
Attach the given dimension to new geometry
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
DatumAxisBuilder.setGeometryAndConstraints(DisplayableObject geometry1,
DatumAxisBuilder.ConstraintType geometryConstraintType1,
int constraintAttribute1,
double constraintValue1,
String constraint1,
DisplayableObject geometry2,
DatumAxisBuilder.ConstraintType geometryConstraintType2,
int constraintAttribute2,
double constraintValue2,
String constraint2,
Sense direction)
Sets two different geometric objects.
|
void |
DatumPlaneBuilder.setGeometryAndConstraints(DisplayableObject geometry1,
DatumPlaneBuilder.ConstraintType geometryConstraintType1,
int constraintAttribute1,
double constraintValue1,
String constraint1,
DisplayableObject geometry2,
DatumPlaneBuilder.ConstraintType geometryConstraintType2,
int constraintAttribute2,
double constraintValue2,
String constraint2)
Sets two different geometric objects.
|
void |
DatumAxisBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumAxisBuilder.CurveOption option,
DisplayableObject secondGeometry,
ICurve curve)
Sets Curve or Edge object and arc length with an extra geometry in picture
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
DatumAxisBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumAxisBuilder.CurveOption option,
ICurve curve,
DisplayableObject secondGeometry)
Sets Curve or Edge object and arc length with an extra geometry in picture
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
void |
DatumPlaneBuilder.setPointOnCurve(double arcLength,
String constraint,
DatumPlaneBuilder.CurveOption option,
ICurve curve,
DisplayableObject secondGeometry)
Sets curve or edge object and arc length with other geometry selected.
|
void |
BooleanBuilder.setTool(DisplayableObject tool)
Deprecated.
Deprecated in NX5.0.2. Use
Features.BooleanBuilder#setToolBodyCollector instead.
|
Modifier and Type | Field and Description |
---|---|
DisplayableObject[] |
StiffenerBuilder.CreatePathData.faces
The faces/datums defining the placement of the profile that is being oriented.
|
Modifier and Type | Method and Description |
---|---|
void |
StandardPartItemBuilder.addAcrossObject(DisplayableObject acrossObject)
Adds the specific object to the across object list.
|
void |
StandardPartItemBuilder.addDeselectedAcrossObject(DisplayableObject acrossObject)
Adds the specific object to the deselected across object list.
|
void |
SplitStandardPartBuilder.convertObjectsToAdd(DisplayableObject[] selectedObjectTags)
Converts the selected objects to acceptable one and add to the selection list.
|
void |
SplitStandardPartBuilder.convertObjectsToRemove(DisplayableObject[] selectedObjectTags)
Converts the selected objects to acceptable one and remove it from the selection list.
|
void |
StandardPartItemBuilder.convertReferenceGeometry(int index,
DisplayableObject selObj)
Converts the selected reference geometry.
|
String |
ManufacturingPreparationBuilder.getDesignElementAttributeValue(DisplayableObject designElement,
ManufacturingPreparationBuilder.AttributeType attrType)
Get the attribute value of the given design element.
|
void |
ManufacturingPreparationBuilder.initializeDesignElementAttributes(DisplayableObject designElement)
Read the design attributes and use them to initialize the builder values.
|
void |
StandardPartItemBuilder.removeAcrossObject(DisplayableObject acrossObject)
Removes the specific object from the across object list.
|
void |
StandardPartItemBuilder.removeDeselectedAcrossObject(DisplayableObject acrossObject)
Removes the specific object from the deselected across object list.
|
void |
ManufacturingPreparationBuilder.setDesignElementAttributeValue(DisplayableObject designElement,
ManufacturingPreparationBuilder.AttributeType attrType,
String attrValue)
Set the attribute value of the given design element.
|
void |
StandardPartItemBuilder.setOptionalGeometry(DisplayableObject selectedGeometry)
Sets one geometry for input selection which has multiple options.
|
void |
OrientationDefinitionBuilder.setPlacementFaces(DisplayableObject[] faces)
Sets the faces or datum that are being processed into the builder.
|
void |
StandardPartItemBuilder.setTransitionGeometry(int index,
DisplayableObject transitionGeometry)
Sets the transition geometry given the index.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionSplitFaceBuilder.addSplitPoint(Point3d location,
DisplayableObject object)
Add split face point.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Field
Represents an Field abstract class.
|
interface |
FieldExpression
Represents the Field Expression class.
|
interface |
FieldFormula
Represents the Field Formula class.
|
interface |
FieldLink
Represents the Field Link class.
|
interface |
FieldReference
Represents an reference field
A Reference Field exposes data inside of an abstract data store. |
Modifier and Type | Interface and Description |
---|---|
interface |
AnalysisObject
Represents an Analysis Object
This is an abstract class, and cannot be instantiated . |
interface |
CurveContinuity
Represents a Curve Continuity Analysis builder
To create or edit an instance of this class, use CurveContinuityBuilder Created in NX7.0.0 |
interface |
CurveCurvatureAnalysis
Represents a CurveCurvatureAnalysis builder
To create or edit an instance of this class, use CurveCurvatureAnalysisBuilder Created in NX7.0.0 |
interface |
DeviationGauge
Deviation Gauge analysis object class
To create or edit an instance of this class, use DeviationGaugeBuilder Created in NX6.0.0 |
interface |
DraftAnalysis
Represents a Draft Analysis builder
To create or edit an instance of this class, use DraftAnalysisBuilder Created in NX8.0.0 |
interface |
FaceCurvatureAnalysis
Represents a Face Curvature Analysis builder
To create or edit an instance of this class, use FaceCurvatureAnalysisBuilder Created in NX8.0.0 |
interface |
GapFlushness
Gap and Flushness analysis object class
To create or edit an instance of this class, use GapFlushnessBuilder Created in NX5.0.0 |
interface |
HighlightLinesAnalysis
Represents a Highlight Lines Analysis object.
|
interface |
LocalRadiusAnalysis
Builder for Local Radius Analysis (formerly Dynamic Radius)
To create or edit an instance of this class, use LocalRadiusAnalysisBuilder Created in NX8.5.0 |
interface |
SectionAnalysisObject
Represents a Section Analysis object.
|
interface |
SurfaceContinuityAnalysis
Represents a SurfaceContinuityAnalysis builder
To create or edit an instance of this class, use SurfaceContinuityAnalysisBuilder Created in NX6.0.0 |
interface |
SurfaceIntersection
Represents a SurfaceIntersection builder
To create or edit an instance of this class, use SurfaceIntersectionBuilder Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
CurveContinuityBuilder |
AnalysisObjectCollection.createCurveContinuityBuilder(DisplayableObject ccaoObject)
Creates a Curve Continuity Builder
License requirements: studio_analyze ("STUDIO ANALYZE") . |
CurveCurvatureAnalysisBuilder |
AnalysisObjectCollection.createCurveCurvatureAnalysisBuilder(DisplayableObject caaoObject)
Creates a curve curvature analysis builder
License requirements: gateway ("UG GATEWAY") . |
DeviationGaugeBuilder |
AnalysisObjectCollection.createDeviationGaugeBuilder(DisplayableObject ddaoObject)
Creates a Deviation Gauge Builder
License requirements: solid_modeling ("SOLIDS MODELING") . |
DraftAnalysisBuilder |
AnalysisObjectCollection.createDraftAnalysisBuilder(DisplayableObject daoObject)
Creates a draft analysis builder
License requirements: studio_analyze ("STUDIO ANALYZE") . |
FaceCurvatureAnalysisBuilder |
AnalysisObjectCollection.createFaceCurvatureAnalysisBuilder(DisplayableObject fcaoObject)
Creates a face curvature analysis builder
License requirements: studio_analyze ("STUDIO ANALYZE") . |
HighlightLinesAnalysisBuilder |
AnalysisObjectCollection.createHighlightLinesAnalysisBuilder(DisplayableObject hpaoObject)
Creates a Highlight Lines Analysis builder
License requirements: studio_analyze ("STUDIO ANALYZE") . |
SurfaceContinuityAnalysisBuilder |
AnalysisObjectCollection.createSurfaceContinuityAnalysisBuilder(DisplayableObject scaoObject)
Creates a surface continuity analysis builder
License requirements: gateway ("UG GATEWAY") . |
SurfaceIntersectionBuilder |
AnalysisObjectCollection.createSurfaceIntersectionBuilder(DisplayableObject siaoObject)
Creates a surface intersection builder
License requirements: studio_analyze ("STUDIO ANALYZE") . |
void |
DraftAnalysisBuilder.deselectFaces(DisplayableObject[] faces)
Deselects faces
License requirements: studio_analyze ("STUDIO ANALYZE") . |
void |
DraftAnalysisBuilder.removeLabelParents(DisplayableObject[] parents)
Removes dynamic label parents
License requirements: studio_analyze ("STUDIO ANALYZE") . |
void |
FaceCurvatureAnalysisBuilder.reverseIndividualNormal(DisplayableObject face)
Reverses an individual face normal.
|
void |
DraftAnalysisBuilder.reverseNormal(DisplayableObject face)
Reverses individual face normal
License requirements: studio_analyze ("STUDIO ANALYZE") . |
void |
DraftAnalysisBuilder.setDynamicParent(int index,
DisplayableObject parent)
Sets dynamic parent
License requirements: studio_analyze ("STUDIO ANALYZE") . |
void |
SurfaceAnalysisDisplay.setShowFlag(DisplayableObject surface,
SurfaceAnalysisDisplay.ShowFlagType choice,
boolean on)
Sets show flags
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
SurfaceContinuityAnalysisBuilder.updateFirstEdgeFace(DisplayableObject edgeOrFace,
Point3d selectionPoint)
The user selects or deselects first edge or face, update builder m_edge1, m_face1
License requirements: gateway ("UG GATEWAY") . |
void |
SurfaceContinuityAnalysisBuilder.updateSecondEdgeFace(DisplayableObject edgeOrFace,
Point3d selectionPoint)
User selects or deselects second edge or face, update builder m_edge2, m_face2
License requirements: gateway ("UG GATEWAY") . |
Modifier and Type | Interface and Description |
---|---|
interface |
SectionAnalysisExObject
Represents a Section Analysis Object of the new version.
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject |
EntityUsageInfo.entity()
Returns the important entity.
|
DisplayableObject |
SupportPlaneData.existingPlane()
Returns the existing face or plane
License requirements: None. |
DisplayableObject[] |
ParentEquivalencyMap.getEntitiesFromCurrentObject()
Get the mapped entities from the current object.
|
DisplayableObject[] |
ParentEquivalencyMap.getEntitiesFromReplacementObject()
Get the mapped entities from the replacement object
License requirements: None. |
DisplayableObject |
Extend.target()
Returns the extend target for the following types
Extend.ExtendType.UNTIL_SELECTED . |
Modifier and Type | Method and Description |
---|---|
void |
SupportPlaneData.setExistingPlane(DisplayableObject existingPlane)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR cam_base ("CAM BASE") . |
void |
ParentEquivalencyMap.setMappedEntities(DisplayableObject[] oldEntities,
DisplayableObject[] newEntities)
Set externally mapped entities
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
ParentEquivalencyMap.setMappedEntities(DisplayableObject[] oldEntities,
DisplayableObject[] newEntities)
Set externally mapped entities
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
ReplAsstBuilder.setNewParents(DisplayableObject[] replacementObjects)
Set the source entities for the Replacement Assistant.
|
void |
Extend.setTarget(DisplayableObject selectedObject)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Modifier and Type | Method and Description |
---|---|
void |
LayerManager.applyMoveToLayerToOwningParts(int newLayer,
DisplayableObject[] objectArray)
Move the selected objects to the specified layer in their Owning Parts.
|
void |
LayerManager.moveDisplayableObjects(int newLayer,
DisplayableObject[] objectArray)
Moves displayable objects to the specified layer.
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
ComponentDefinition.getMembers(Layout2dComponentMemberType memberType)
Returns an array of specified members in this component definition
License requirements: nx_layout ("NX Layout") . |
DisplayableObject[] |
Component.getMembers(Layout2dComponentMemberType memberType)
Returns an array of specified members in this component
License requirements: nx_layout ("NX Layout") . |
Modifier and Type | Method and Description |
---|---|
void |
Component.addExistingCurves(DisplayableObject[] curves)
Add an array of specified curves from top level sketch to this component
License requirements: nx_layout ("NX Layout") . |
boolean |
ComponentCollection.isComponentMember(DisplayableObject disObject)
Verify if the object belong to this component
License requirements: nx_layout ("NX Layout") . |
Modifier and Type | Method and Description |
---|---|
DisplayableObject |
MarkupObject.anchorObject()
Returns the anchor object
License requirements: None. |
DisplayableObject[] |
MarkupObject.getAssociatedObjects()
Gets the associated objects
License requirements: None. |
DisplayableObject[] |
MarkupObject.getTerminatingObjects()
Gets the terminating objects
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
MarkupObject.setAnchorObject(DisplayableObject anchorObj)
License requirements: None. |
void |
MarkupObject.setAssociatedObjects(DisplayableObject[] associatedObjects)
Sets the associated objects
License requirements: None. |
void |
MarkupObject.setTerminatingObjects(DisplayableObject[] terminatingObjs)
Sets the terminating objects
License requirements: None. |
Modifier and Type | Interface and Description |
---|---|
interface |
AdapterSignal
Represents the Adapter Signal class.
|
interface |
AngularLimitJoint
Represents the Angular Limit Joint.
|
interface |
AngularSpringJoint
Represents the Angular Spring Joint.
|
interface |
BallJoint
Represents the Ball Joint.
|
interface |
BreakingConstraint
Represents the Breaking Constraint.
|
interface |
Cam
Represents the Cam Constraint.
|
interface |
ChangeMaterial
Represents the Change material constraint.
|
interface |
CollisionBody
Represents the Collision Body class.
|
interface |
CollisionSensor
Represents the Collision Sensor.
|
interface |
Coupling
Represents the mechatronics coupling class.
|
interface |
CurveOnCurveJoint
Represents the CurveOnCurve Joint.
|
interface |
CylindricalJoint
Represents the Cylindrical Joint.
|
interface |
DisplayChanger
Represents the Display Changer which is used to change the display properties (Color, Translucency, and Visibility)
of rigid body during simulation.
|
interface |
FixedJoint
Represents the Fixed Joint.
|
interface |
Gear
Represents the Gear.
|
interface |
GraphControl
Represents the Graph Control.
|
interface |
HingeJoint
Represents the Hinge Joint.
|
interface |
LinearLimitJoint
Represents the Linear Limit Joint.
|
interface |
LinearSpringJoint
Represents the Linear Spring Joint.
|
interface |
ObjectSink
Represents the Object Sink.
|
interface |
ObjectSource
Represents the Object Source.
|
interface |
ObjectTransformer
Represents the Object Transformer.
|
interface |
PathConstraintJoint
Represents the Path Constraint Joint class.
|
interface |
PhysicsConstraint
Represents the mechatronics constraint class.
|
interface |
PhysicsJoint
Represents the mechatronics joint class.
|
interface |
PointOnCurveJoint
Represents the PointOnCurve Joint.
|
interface |
PositionControl
Represents the Position Control.
|
interface |
PreventCollision
Represents the Prevent Collision Constraint.
|
interface |
ProxyObject
Represents the Proxy Object class.
|
interface |
RigidBody
Represents the Rigid Body class.
|
interface |
SignalAdapter
Represents the Signal Adapter class.
|
interface |
SlidingJoint
Represents the Sliding Joint.
|
interface |
SpeedControl
Represents the Speed Control.
|
interface |
SpringDamper
Represents the Spring Damper.
|
interface |
TransportSurface
Represents the Transport Surface class.
|
Modifier and Type | Method and Description |
---|---|
void |
PreventCollisionBuilder.setFirstBody(DisplayableObject firstBody)
Sets the first object.
|
void |
ChangeMaterialBuilder.setFirstBody(DisplayableObject firstBody)
Sets the first object.
|
void |
PreventCollisionBuilder.setSecondBody(DisplayableObject secondBody)
Sets the second object.
|
void |
ChangeMaterialBuilder.setSecondBody(DisplayableObject secondBody)
Sets the second object.
|
Modifier and Type | Interface and Description |
---|---|
interface |
BodyContact
Represents a
BodyContact
To create or edit an instance of this class, use BodyContactBuilder Created in NX5.0.0 |
interface |
Bushing
Represents a bushing
To create or edit an instance of this class, use BushingBuilder Created in NX6.0.0 |
interface |
Connector
Represents a connector
This is an abstract class, and cannot be created. |
interface |
Coupler
Represents a motion coupler object
This is an abstract class, and cannot be created. |
interface |
CouplerCable
Represents a motion cable object
To create or edit an instance of this class, use CouplerCableBuilder Created in NX6.0.0 |
interface |
CouplerGear
Represents a motion gear object
To create or edit an instance of this class, use CouplerGearBuilder Created in NX6.0.0 |
interface |
CouplerRckpn
Represents a motion rack and pinion object
To create or edit an instance of this class, use CouplerRckpnBuilder Created in NX6.0.0 |
interface |
CurveContact
Represents a
CurveContact
To create or edit an instance of this class, use CurveContactBuilder Created in NX5.0.0 |
interface |
CurveOnCurve
Represents a curve on curve
To create or edit an instance of this class, use CurveOnCurveBuilder Created in NX6.0.0 |
interface |
Damper
Represents a damper
To create or edit an instance of this class, use DamperBuilder Created in NX6.0.0 |
interface |
FlexBody
Represents the Motion FlexBody class.It must be associated
with a Motion Link.
|
interface |
GeneralCoupler
Represents motion 2-3 joint coupler
To create or edit an instance of this class, use GeneralCouplerBuilder Created in NX7.5.0 |
interface |
Joint
Represents a motion joint object
To create or edit an instance of this class, use JointBuilder Created in NX5.0.0 |
interface |
Link
Represents the Motion Link class.
|
interface |
LoadTransfer
Represents a Motion Load Transfer class
To create or edit an instance of this class, use LoadTransferBuilder Created in NX9.0.0 |
interface |
Marker
Represents the Motion Marker class.
|
interface |
MotionObject
Represents the motion base object class.
|
interface |
MotionSensor
Represents a motion sensor
To create or edit an instance of this class, use MotionSensorBuilder Created in NX6.0.0 |
interface |
Motor
Represents a motion motor base object class
This is an abstract class, and cannot be created. |
interface |
PMDCMotor
Represents a motion pmdc motor object
To create or edit an instance of this class, use PMDCMotorBuilder Created in NX6.0.0 |
interface |
PointOnCurve
Represents a point on curve
To create or edit an instance of this class, use PointOnCurveBuilder Created in NX6.0.0 |
interface |
PointOnSurface
Represents a point on surface motion object
To create or edit an instance of this class, use PointOnSurfaceBuilder Created in NX6.0.0 |
interface |
ScalarForce
Represents the Motion ScalarForce class.
|
interface |
ScalarTorque
Represents the Motion ScalarTorque class.
|
interface |
Spring
Represents a spring
To create or edit an instance of this class, use SpringBuilder Created in NX6.0.0 |
interface |
VectorForce
Represents a vector force
To create or edit an instance of this class, use VectorForceBuilder Created in NX5.0.0 |
interface |
VectorTorque
Represents a vector torque
To create or edit an instance of this class, use VectorTorqueBuilder Created in NX5.0.0 |
Modifier and Type | Field and Description |
---|---|
DisplayableObject |
PackagingMeasureBuilder.GeometryData.geometry
Geometry
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
PackagingBuilder.getList1()
Returns geometry list 1 of
Packaging object. |
DisplayableObject[] |
PackagingMeasureBuilder.getList2()
Returns the geometry list 2 of
PackagingMeasure object. |
DisplayableObject[] |
PackagingInterferenceBuilder.getList2()
Gets the geometry list 2 of
PackagingInterference object. |
DisplayableObject[] |
PackagingTraceBuilder.getRelativeLinks()
Returns
PackagingTrace relative links. |
DisplayableObject[] |
PackagingInterferenceBuilder.getRelativeLinks()
Returns
PackagingInterference user selected relative links. |
Modifier and Type | Method and Description |
---|---|
void |
PackagingBuilder.setList1(DisplayableObject[] list1)
Sets geometry list 1.
|
void |
PackagingMeasureBuilder.setList2(DisplayableObject[] list2)
Sets the geometry list 2.
|
void |
PackagingInterferenceBuilder.setList2(DisplayableObject[] list2)
Sets the geometry list 2 of
PackagingInterference object. |
void |
PackagingTraceBuilder.setRelativeLinks(DisplayableObject[] links)
Sets
PackagingTrace relative links. |
void |
PackagingInterferenceBuilder.setRelativeLinks(DisplayableObject[] links)
Sets
PackagingInterference user selected relative links. |
Constructor and Description |
---|
GeometryData(DisplayableObject geometryInitial,
Point3d pointInitial,
Vector3d vectorInitial,
nxopen.Direction directionInitial)
Constructor for the GeometryData object.
|
Modifier and Type | Interface and Description |
---|---|
interface |
DisplayedConstraint
The displayed representation of a constraint, used for graphical
display and to represent it in the Assembly Navigator.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Anchor
A Routing Anchor defines a position in a Qualified Routing component part.
|
interface |
ArcSegment
Represents a arc segment.
|
interface |
ControlPoint
Routing Control Points define a position in space, and are used to determine connections
from segments to segments, and segments to ports.
|
interface |
FormboardFrame
The
FormboardFrame is a (not pure) virtual class. |
interface |
FormboardFrameCGM
Represents a Formboard Frame CGM.
|
interface |
FormboardFramePattern
Represents a Formboard Frame Pattern.
|
interface |
FormboardFrameRectangle
Represents a Formboard Frame Rectangle.
|
interface |
GapArcSegment
Represents a gap arc segment.
|
interface |
LineSegment
Represents a line segment.
|
interface |
SplineSegment
Represents a spline segment.
|
Modifier and Type | Field and Description |
---|---|
DisplayableObject |
FormboardFrame.ObjectData.geometry
Underlying geometry
|
DisplayableObject |
FormboardFrameCollection.ImportPatternData.group
returning the geometry of imported file
|
Modifier and Type | Method and Description |
---|---|
ISegment |
SegmentManager.createHealSpline(DisplayableObject startObject,
DisplayableObject endObject,
HealPath healPath)
Creates a spline
ISegment object
with input ControlPoint as ends. |
Modifier and Type | Interface and Description |
---|---|
interface |
DieEngTrimAngleCheck
Represents a die engineering trim angle check analysis object
To create or edit an instance of this class, use DieEngTrimAngleCheckBuilder Created in NX8.5.0 |
Modifier and Type | Method and Description |
---|---|
FlowDisplayBuilder |
MoldDesignCollection.createFlowDisplayBuilder(DisplayableObject moldex3DResult)
Creates flow display builder
License requirements: ug_mold_design ("UG MOLD") . |
Modifier and Type | Interface and Description |
---|---|
interface |
UserDefinedObject
JA interface for the UserDefinedObject object .
|
Modifier and Type | Field and Description |
---|---|
DisplayableObject[] |
WeldPointBuilder.FaceSetData.objects
the face set reference objects
|
Modifier and Type | Method and Description |
---|---|
DisplayableObject[] |
WeldPointBuilder.getMirrorTranslateReferenceObjects()
Get mirror translate reference objects
License requirements: ugweld ("UG WELD") . |
Modifier and Type | Method and Description |
---|---|
void |
WeldPointBuilder.setFaceSet(WeldFacesetIndex facesetIndex,
DisplayableObject[] objects)
Sets the user selected faces for the indicated face set
License requirements: ugweld ("UG WELD") . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.