Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static DisplayManager.LayerSetting |
DisplayManager.LayerSetting.CHANGE_LAYER_TO_SELECTABLE
Change the layer to selectable if it is invisible
|
static DisplayManager.LayerSetting |
DisplayManager.LayerSetting.INVALID
Last value, should not be used.
|
static DisplayManager.LayerSetting |
DisplayManager.LayerSetting.MOVE_OBJECTS_TO_WORK_LAYER
Move the objects to work layer if they are in invisible layer
|
Modifier and Type | Method and Description |
---|---|
static DisplayManager.LayerSetting |
DisplayManager.LayerSetting.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayManager.LayerSetting |
DisplayManager.LayerSetting.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayManager.LayerSetting[] |
DisplayManager.LayerSetting.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DisplayManager.showObjects(DisplayableObject[] objects,
DisplayManager.LayerSetting layerSetting)
Unblank a set of displayable objects considering the following layer settings if the objects are in invisible layers.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.