Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Method and Description |
---|---|
CutView |
CutViewCollection.findObject(String journalIdentifier)
Finds the
CutView with the given identifier
as recorded in a journal. |
Modifier and Type | Method and Description |
---|---|
ModelingView |
CutViewCollection.createLinkedSectionView(CutView view)
Create a linked section view.
|
void |
CutViewCollection.deleteCutView(CutView view)
Delete the Master Cut feature associated with a cut view.
|
CutViewCollection.IsCutBodyOfViewData |
CutViewCollection.isCutBodyOfView(Body body,
CutView view)
Return a "true" if the body is a cut body in the view.
|
CutViewCollection.IsUncutBodyOfViewData |
CutViewCollection.isUncutBodyOfView(Body body,
CutView view)
Return a "true" if the body is an uncut body in the view.
|
void |
CutViewCollection.updateCutView(CutView view)
Update the Master Cut feature associated with a cut view.
|
Modifier and Type | Method and Description |
---|---|
boolean |
FeatureCollection.getIsMasterCutVisibleInView(Feature masterCut,
CutView view)
Returns if a
MasterCutBuilder is visbible in specified CutView . |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.