Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static CGMBuilder.SizeOption |
CGMBuilder.SizeOption.DIMENSION
Dimension, uses the units along with X and Y dimensions to determine CGM size
|
static CGMBuilder.SizeOption |
CGMBuilder.SizeOption.FULL_SCALE
Full Scale
|
static CGMBuilder.SizeOption |
CGMBuilder.SizeOption.SCALE_FACTOR
Scale Factor, scales the CGM based on user defined scale field
|
Modifier and Type | Method and Description |
---|---|
CGMBuilder.SizeOption |
CGMBuilder.size()
Returns the size of the CGM.
|
static CGMBuilder.SizeOption |
CGMBuilder.SizeOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CGMBuilder.SizeOption |
CGMBuilder.SizeOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CGMBuilder.SizeOption[] |
CGMBuilder.SizeOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CGMBuilder.setSize(CGMBuilder.SizeOption size)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.