Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static CGMBuilder.MultipleOption |
CGMBuilder.MultipleOption.INDIVIDUAL
Save Multiple sheets as individual CGMs
|
static CGMBuilder.MultipleOption |
CGMBuilder.MultipleOption.SINGLE
Save Multiple sheets as one CGM
|
Modifier and Type | Method and Description |
---|---|
CGMBuilder.MultipleOption |
CGMBuilder.multiple()
Returns the multiple option is used when more than one drawing is exported.
|
static CGMBuilder.MultipleOption |
CGMBuilder.MultipleOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CGMBuilder.MultipleOption |
CGMBuilder.MultipleOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CGMBuilder.MultipleOption[] |
CGMBuilder.MultipleOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CGMBuilder.setMultiple(CGMBuilder.MultipleOption multiple)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.