Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static CGMBuilder.ActionOption |
CGMBuilder.ActionOption.CREATE_NEW
Creates a new dataset in Teamcenter
|
static CGMBuilder.ActionOption |
CGMBuilder.ActionOption.FILE_BROWSER
Option allows for export of CGM file to local location when running Teamcenter
|
static CGMBuilder.ActionOption |
CGMBuilder.ActionOption.OVERWRITE_EXISTING
Overwrites an existing dataset in Teamcenter
|
Modifier and Type | Method and Description |
---|---|
CGMBuilder.ActionOption |
CGMBuilder.action()
Returns the action option to be used when exporting the CGM file when in Teamcenter
mode.
|
static CGMBuilder.ActionOption |
CGMBuilder.ActionOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static CGMBuilder.ActionOption |
CGMBuilder.ActionOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static CGMBuilder.ActionOption[] |
CGMBuilder.ActionOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
CGMBuilder.setAction(CGMBuilder.ActionOption action)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.