Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AxisOrientation |
AxisOrientation.HORIZONTAL |
AxisOrientation |
Sketch.ReferenceDirectionData.referenceAxisOrientation
Indicates whether the reference axis is horizontal or vertical
|
static AxisOrientation |
AxisOrientation.VERTICAL |
Modifier and Type | Method and Description |
---|---|
AxisOrientation |
SketchInPlaceBuilder.axisOrientation()
Returns the reference axis orientation (horizontal or vertical)
License requirements: None. |
static AxisOrientation |
AxisOrientation.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AxisOrientation |
AxisOrientation.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AxisOrientation[] |
AxisOrientation.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
Sketch |
SketchCollection.createSketch(String name,
ISurface attachmentPlane,
IReferenceAxis referenceAxis,
Vector3d referenceDirection,
AxisOrientation referenceAxisOrientation,
Sense referenceAxisSense,
PlaneNormalOrientation normalOrientation)
Deprecated.
Deprecated in NX7.5.3. Use
SketchInPlaceBuilder instead.
|
Sketch |
SketchCollection.createSketch(String name,
ISurface attachmentPlane,
IReferenceAxis referenceAxis,
Vector3d referenceDirection,
AxisOrientation referenceAxisOrientation,
Sense referenceAxisSense,
PlaneNormalOrientation normalOrientation,
NXObject view)
Deprecated.
Deprecated in NX7.5.3. Use
SketchInDraftingBuilder instead.
|
void |
Sketch.reattach(ISurface attachmentPlane,
IReferenceAxis referenceAxis,
Vector3d referenceDirection,
AxisOrientation referenceAxisOrientation,
Sense referenceAxisSense,
PlaneNormalOrientation normalOrientation,
Point3d localCoordinateSystemOrigin)
Reattaches a sketch.
|
void |
SketchInPlaceBuilder.setAxisOrientation(AxisOrientation axisOrientation)
License requirements: None. |
void |
Sketch.setReferenceDirection(IReferenceAxis referenceAxis,
Vector3d referenceDirection,
AxisOrientation referenceAxisOrientation,
Sense referenceAxisSense)
Sets the reference direction of the sketch.
|
Modifier and Type | Method and Description |
---|---|
Note |
AnnotationManager.createNote(String[] textLines,
Point3d origin,
AxisOrientation orientation,
LetteringPreferences letteringPreferences,
UserSymbolPreferences userSymbolPreferences)
Creates a note
License requirements: drafting ("DRAFTING") . |
Modifier and Type | Field and Description |
---|---|
AxisOrientation |
RPOBuilder.ReferenceDirectionData.orientation
Orientation of reference
|
Modifier and Type | Method and Description |
---|---|
void |
RPOBuilder.setReferenceDirection(nxopen.IReferenceAxis reference,
AxisOrientation orientation)
Sets a horizontal or vertical reference for the feature.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.